Skip to main content
Associate
January 20, 2024
Solved

stm32 ADC scann mdoe

In the ADC scan mode in STM32 microcontrollers, the digitized value of all input channels is dumped into ADCx->DR. Is there a register or flags to find out which ADC channel the data currently in the ADCx->DR register

```

void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
 if(hadc->Instance == ADC1)
 {
 uint16_t adc_data;
 
 // Read the converted data from the ADC data register
 adc_data = ADC1->DR; //I don't know which ADC channel this data is related to
 
 // Process the ADC data as needed
 // ...
 }
}

void ADC_Init()
{
 ADC_ChannelConfTypeDef sConfig;

 hadc.Instance = ADC1;
 hadc.Init.ScanConvMode = ENABLE;
 hadc.Init.ContinuousConvMode = ENABLE;
 hadc.Init.NbrOfConversion = 2; // Number of channels to convert
 hadc.Init.DiscontinuousConvMode = DISABLE;
 hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc.Init.NbrOfDiscConversion = 1;
 if (HAL_ADC_Init(&hadc) != HAL_OK)
 {
 Error_Handler();
 }

 // Configure the ADC channels to be converted
 sConfig.Channel = ADC_CHANNEL_0;
 sConfig.Rank = 1;
 sConfig.SamplingTime = ADC_SAMPLETIME_13CYCLES_5;
 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = 2;
 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
}
This topic has been closed for replies.
AScha.3
AScha.3Best answer
Super User
January 20, 2024

You set up the sequence, the ADC is converting - right ?

So you should know , whats the first channel/result and whats the next - and so on.

Results are coming just in the sequence order, you set up - so if you set sequence to convert 

ch1 - ch3 - ch4  the results are for ch1 - ch3 - ch4 -  ch1 - ch3 - ch4  ....      . Thats it.

If you feel a post has answered your question, please click on " Best Answer ".

4 replies

AScha.3
AScha.3Best answer
Super User
January 20, 2024

You set up the sequence, the ADC is converting - right ?

So you should know , whats the first channel/result and whats the next - and so on.

Results are coming just in the sequence order, you set up - so if you set sequence to convert 

ch1 - ch3 - ch4  the results are for ch1 - ch3 - ch4 -  ch1 - ch3 - ch4  ....      . Thats it.

If you feel a post has answered your question, please click on " Best Answer ".
Associate
January 21, 2024

Yes, I know the order of the channels, but suppose for some reason  ADC interrupt does not run (for example, due to the occurrence of a simultaneous interrupt with a higher priority). After that, we may not be able to distinguish which channel the current data belongs to

AScha.3
Super User
January 21, 2024

No, still the next value you get/read , is the next in the sequence.

You always do only one conversion, then read the result.

So give high enough priority to the adc interrupt , to be sure, you can keep the speed, you want.

 

Or do the (adc sequence) -> [data array]  with the DMA, then you cannot have problems about loosing a result (and the "position" in the sequence). For using the adc at hi speed and/or big array of results you should use the DMA anyway.

ed.:

from F1 rm :

AScha3_0-1705846122968.png

So if using the sequence scan mode, you need to use dma anyway and so always sequence is stored correct .

If you feel a post has answered your question, please click on " Best Answer ".