Skip to main content
VK Verma
Associate III
May 8, 2023
Question

STLinkV3-Mods debug error " remote failure reply E3" , I have updated its firmware with STM32CubeProgramer successfully with version V3J10M3B5S1 but still problem persist

..

This topic has been closed for replies.

3 replies

ST Technical Moderator
May 8, 2023

Hello @VK Verma​ ,

Which device used ?

Check "Connect under reset" options, or BOOT0=HIGH settings.

Check configuration of pins used by the debug interface.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
VK Verma
VK VermaAuthor
Associate III
May 9, 2023

Hi Imen,

Thanks for your reply,

As far hardware side is concerned the same hardware at SWD connector is debugable with STLink Version V3 Set and STLink V2 but not with STLinkV3 Mods tool.

and with Connect under rest setting.

I will still reverify the cable from STLinkV3 Mods to the target board.

Regards,

Vk Verma

VK Verma
VK VermaAuthor
Associate III
May 9, 2023

Hi Imen,

I finally able to find the problem, it is with the SWD cable. I used core cable type having 8 signal wires in one core which might be causing single transmission issues but the same cable was working with other st link tool. After replacing it with FRC Cable the STlink Mods is working fine.

Can you please suggest "What is the maximum length of SWD cable be used with STlink V3 Mods"

Regards,

VK Verma