Skip to main content
CBier.1
Associate II
November 2, 2025
Solved

STLINK-V3MODS – Bridge GPIOs won’t work as Outputs

Hi everyone,

I’m trying to use the STLINK-V3MODS Bridge GPIOs (GPIO0–GPIO3) as digital outputs, but none of them show any voltage change at the pins — not even in Open-Drain mode with an external pull-up.

All API calls (InitGPIO / SetResetGPIO / ReadGPIO) report BRG_NO_ERR,
but on the hardware side, the GPIO pins stay flat at 0 V regardless of the configuration or the logical state set.

 

🧩 Setup

 

:gear: What I did

  • Used InitGPIO() + SetResetGPIO()

  • Tried both Push-Pull and Open-Drain modes

  • T_VCC is connected (3.3 V detected)

  • Closed all COMs between runs (CloseBridge(COM_UNDEF_ALL))

Result:

  • Software side → success (BRG_NO_ERR, errMask = 0x00)

  • Hardware side → no voltage change, always 0 V

  • Tried with LED + 1 kΩ to 3.3 V, tried external 10 kΩ pull-up — no visible switching

It looks like the Bridge GPIOs are either disabled in firmware, or blocked by the internal level-shifters.

 

:question_mark: Questions to ST / community

  1. Are Bridge GPIOs on STLINK-V3MODS truly open-drain only (through level-shifters)?

  2. Has anyone measured an actual sourcing HIGH at CN2 pins in Push-Pull mode?

  3. Any official documentation (UM/AppNote) confirming this hardware behavior?

CBier.1
CBier.1Best answer
Associate II
November 10, 2025

I found a solution how to get it working. In my example i always closed the connection. this leads to the fact, that the Pins are lost there state. If you delete:

 // Cleanup
 cli.Disconnect();
 if (brg) { brg->CloseBridge(COM_UNDEF_ALL); brg->CloseStlink(); delete brg; }
 if (pIf) { delete pIf; }

this in the code, the status of the pins will be not changed 

2 replies

AScha.3
Super User
November 2, 2025

Hi,

i never played with the bridge on V3mods, but from bridge.cpp :

// GPIO 0, 1, 2, 3 config, Bit1-0 mode, Bit3-2 speed, Bit5-4 pull, Bit6 output type

and xx.h :

/// GPIO port mode configuration, see also \ref LIMITATION
typedef enum {
	GPIO_MODE_INPUT = 0, ///< Input mode
	GPIO_MODE_OUTPUT = 1, ///< Ouptput mode
	GPIO_MODE_ANALOG = 3 ///< Analog mode
}Brg_GpioModeT;

/// GPIO port output speed configuration
typedef enum {
	GPIO_SPEED_LOW = 0, ///< Low speed
	GPIO_SPEED_MEDIUM = 1, ///< Medium speed
	GPIO_SPEED_HIGH = 2, ///< High speed
	GPIO_SPEED_VERY_HIGH = 3 ///< Very high speed
}Brg_GpioSpeedT;

/// GPIO port pull-up/pull-down configuration
typedef enum {
	GPIO_NO_PULL = 0, ///< No pull-up, no pull-down
	GPIO_PULL_UP = 1, ///< Pull-up
	GPIO_PULL_DOWN = 2 ///< Pull-down
}Brg_GpioPullT;

/// GPIO port output type configuration
typedef enum {
	GPIO_OUTPUT_PUSHPULL = 0, ///< Output push-pull
	GPIO_OUTPUT_OPENDRAIN = 1 ///< Output open-drain
}Brg_GpioOutputT;

/// GPIO init configuration, see also \ref LIMITATION
typedef struct {
	Brg_GpioModeT Mode; ///< GPIO port mode
	Brg_GpioSpeedT Speed; ///< GPIO port output speed
	Brg_GpioPullT Pull; ///< GPIO port pull-up/pull-down
	Brg_GpioOutputT OutputType; ///< GPIO port output type
}Brg_GpioConfT;

/// GPIO init parameters for Brg::InitGPIO(), see also \ref LIMITATION
typedef struct {
	uint8_t GpioMask; ///< GPIO(s) to be configured (one or several value of #Brg_GpioMaskT)
	uint8_t ConfigNb; ///< Number of #Brg_GpioConfT pointed by pGpioConf:\n
	 ///< must be #BRG_GPIO_MAX_NB or 1 (if 1 pGpioConf[0] used for all gpios)
	Brg_GpioConfT *pGpioConf; ///< Table of ConfigNb init configuration.\n
	 ///< If #BRG_GPIO_MAX_NB, pGpioConf[0] for GPIO_0, .., pGpioConf[3] for GPIO_3. \n
	 ///< GPIO(s) that are not present in GpioMask are not configured.
} Brg_GpioInitT;

 

..so pins can be set to in, out, pull..  like any standard i/o pin, depending on : const Brg_GpioInitT *pInitParams .

What you set here ?

If you feel a post has answered your question, please click on " Best Answer ".
CBier.1
CBier.1AuthorBest answer
Associate II
November 10, 2025

I found a solution how to get it working. In my example i always closed the connection. this leads to the fact, that the Pins are lost there state. If you delete:

 // Cleanup
 cli.Disconnect();
 if (brg) { brg->CloseBridge(COM_UNDEF_ALL); brg->CloseStlink(); delete brg; }
 if (pIf) { delete pIf; }

this in the code, the status of the pins will be not changed