Skip to main content
Senior
Jul 31, 2025 8:38 PM UTC
Solved

STLINK V3 stopped working after upgrade

STLINK V3 stopped working after upgrade. Red light is flashing. Device manager - Unknown USB Device. NUCLO and DISCOVERY with ST-Link2 are still working! Installing dpinst_amd64.exe not help.

This topic has been closed for replies.
GS2Best answer
Senior
Jul 31, 2025 9:26 PM UTC

Thanks, I have already removed USB hub. Yes, I replace the cable and it is working now.

Thank you very much. How can upgrade brake the cable?!

5 replies

TDK
Jul 31, 2025 9:12 PM UTC

If red light is flashing, it indicates enumeration is failing. Try a different cable or adding/removing a USB hub from the chain.

"If you feel a post has answered your question, please click ""Accept as Solution""."
GS2AuthorBest answer
Senior
Jul 31, 2025 9:26 PM UTC

Thanks, I have already removed USB hub. Yes, I replace the cable and it is working now.

Thank you very much. How can upgrade brake the cable?!

Tesla DeLorean
Guru
Jul 31, 2025 10:02 PM UTC

Operates at a faster rate, say 480 Mbps vs 12 Mbps, and then the cable quality/performance becomes much more of an issue..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..