Skip to main content
ABric.2
Associate II
June 8, 2023
Question

STLink-V3 MiniE return DEV_TARGET_CMD_ERR

Hi,

I'm using STLink-V3 MiniE tu flash STM32L432CCU6 on custom board.

The signal mapped are SWDIO & SWCLK. I connect T_VCC to 3V3.

The connexions are correct has I was able to flash the target.

I'm using STM32CubeProgrammer CLI, and control the target power supply by software (testbench).

But sometimes, the STLink-V3 MiniE couldn't flash/read target and print DEV_TARGET_CMD_ERR in the log file.

What this error means ? How to avoid it to be able to flash/read every time ?

Best regards,

Antoine

This topic has been closed for replies.

1 reply

ST Technical Moderator
July 3, 2023

Hello @ABric.2 ,

Make sure that the power supply VDD from the application board is properly connected.

Check pins connection following this UM2502  STLINK-V3MODS and STLINK-V3MINI debugger/programmer tiny probes for STM32 microcontrollers - User manual

Hope this helps!

 

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks