Skip to main content
Associate II
Nov 29, 2025 11:49 AM UTC
Question

STEVAL-STWINKT1B: how to send data directly to a nucleo board?

Hardware: STEVAL-STWINKT1B and NUCLEO-N657X0-Q

The STEVAL supports Nano Edge Studio and stdatalog-pysdk , but this will not work when communicating P2P to a Nucleo. Are there example codes for the STEVAL where it communicates eg. via UART to other boards? The only resource I could find is fp-sns-datalog2/Projects/STM32L4R9ZI-STWIN/Applications/DATALOG2 at main · STMicroelectronics/fp-sns-datalog2 , is it difficult to implement a communication protocol using that? There were multiple example codes for the NUCLEO, so no problem there. 

I already have implemented UART IT buffer on Nucleo (struggled getting UART DMA to work), so it would be easiest if something similar could be implemented on STEVAL.

 

1 reply

williskAuthor
Associate II
Dec 5, 2025 11:21 AM UTC

Update: I think i found the correct repo: stm32-hotspot/stm32ai-nanoedge-datalogger: STM32 Application for datalogging feature with NanoEdge AI Studio It claims to show how to print sensor data over UART. I have not tried it yet, will be interesting to see how it works.