Skip to main content
FB__1
Associate III
Jul 17, 2025 6:54 AM UTC
Solved

STEVAL-66GYMAI STM32N6 S-Board (VD66GY) compatibility with STM32N6570-DK

Hello ST,

 

Can you confirm if the hardware of the https://www.st.com/en/evaluation-tools/steval-66gymai.html#overview is compatible with the https://www.st.com/en/evaluation-tools/stm32n6570-dk.html. Can i connect them together with the FCC cable (MIPI-CSI connector) ?


Is this the correct driver https://github.com/STMicroelectronics/x-cube-isp/tree/main/Middlewares/ST/STM32_Camera_Middleware/sensors/vd6g that i should use to work with the VD66GY on the STM32N6.

 

Thank you.

 

This topic has been closed for replies.
AlexWEI
AlexWEIBest answer
ST Employee
Oct 14, 2025 8:25 AM UTC

hi

the STM32N6 currently supported cameras list here:

https://github.com/STMicroelectronics/STM32N6-GettingStarted-SemanticSegmentation/blob/main/Doc/Build-Options.md#cameras-module

in the list V66GY is supported.  the 2 hardware is compatible, you can try to connect the camera with the N6 DK board. 

2 replies

AlexWEI
AlexWEIBest answer
ST Employee
Oct 14, 2025 8:25 AM UTC

hi

the STM32N6 currently supported cameras list here:

https://github.com/STMicroelectronics/STM32N6-GettingStarted-SemanticSegmentation/blob/main/Doc/Build-Options.md#cameras-module

in the list V66GY is supported.  the 2 hardware is compatible, you can try to connect the camera with the N6 DK board. 

FB__1
FB__1Author
Associate III
Oct 14, 2025 11:44 AM UTC

yes, it works with the stm32n6570-dk