Skip to main content
Associate
Sep 11, 2025 4:51 PM UTC
Question

ST32L5-discovery problem with connect to stlink

I try to connect by usb cable via stm32cubeprogrammer to new board but windows not see any st-link interface. older st-link v2 work fine but this on boad interfave not work. 
Com's led light on green and red colour. led 5VLD12 on green display work - whats wrong ?

This topic has been closed for replies.

3 replies

ST Technical Moderator
Sep 12, 2025 12:54 AM UTC

Hello @tomee and welcome to the Community,

Did you try update the ST-Link firmware to the latest version and using STM32CubeProgrammer?

Please check the tips shared in this article: How to solve connection errors when connecting and programming the STM32 target board.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
tomeeAuthor
Associate
Sep 12, 2025 4:28 AM UTC

@Imen.D , 

Thank you for your reply.

I have the latest version of the programmer installed, but when I connect the Discovery board to my Windows system, no device is detected – the programmer also doesn’t recognize it.

However, when I connect my old ST-LINK V2 dongle, both the system and the programmer detect it without any issues. This problem only occurs with the Discovery board.

ST Technical Moderator
Sep 15, 2025 7:05 AM UTC

Hi @tomee,

Maybe you have COM port conflicts!

Check the jumpers on the board and make sure that they are set correctly. 

Did you try connecting under reset mode?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks