Skip to main content
Associate II
July 9, 2024
Question

ST morpho connector on NUCLEO-F030R8

Hi, 

In NUCLEO-F030R8 what is the pitch and overall dimensions for CN7 & CN10 ST Morpho Connector ?

Also which mating connector is used for these two connectors 

This topic has been closed for replies.

2 replies

STTwo-32
ST Technical Moderator
July 9, 2024

Hello @Meghla and welcome to the ST Community :smiling_face_with_smiling_eyes:.

You can find all details about the CN10 and CN7 on the Bill of material of the NUCLEO-F030R8 available on NUCLEO-F030R8 - STM32 Nucleo-64 development board with STM32F030R8 MCU, supports Arduino and ST morpho connectivity - STMicroelectronics (just search for the CN7 or CN10).  Also, you will find all available dimensions on the Figure 5 of the UM1724.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
July 9, 2024

It's just a standard 0.1" pitch

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.