Skip to main content
parth kothiya
Associate III
April 8, 2022
Question

ST-LINK V3 MODS not connect with target device STM32F0.

I have recently purchase ST-LINK V3 MODS

I am trying to connect it using SWD protocol using STM32CUBE PROGRAMMER software but it gives error DEV_TARGET_CMD_ERR

if i use STLINK V2 then it works fine.

how can i solve this?

is there any connection problem?

my connection pins on ST-LINK V3 MODS

pin no--------function

left side of STLINK V3

4 - T_JTMS/T_SWDIO

8 - GND

13 - T_JCLK/T_SWCLK

right side of STLINK V3

30 - T_Vcc

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
April 8, 2022

Not at 24 MHz, try 1 or 2 MHz

Doesn't have buffers, doesn't need target voltage​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
parth kothiya
Associate III
April 8, 2022

Error: No STM32 target found!

11:43:38 : ST-LINK SN : 0027001F4D46500F20373033

11:43:38 : ST-LINK FW : V3J8M3B5S1

11:43:38 : Board : STLINK-V3MODS

11:43:38 : Voltage : 0.00V

still not connecting

parth kothiya
Associate III
April 8, 2022

out put voltage and current of STLINK V3 is not sufficient for higher clock speed?

i have placed cable to connect my board with STLINK V3 cable length is (30 cm).

how can i increase clock speed of 1-2 MHz.

ST LINK V2 works fine with 4MHz but ST LINK V3 works fine at 5KHz with same board and cable length.