Skip to main content
Associate
June 19, 2023
Question

ST-Link/V2 ISOL can't connect after FW update

Hello,

I was using my ST-Link/V2 ISOL, to reflash some units, but after an update with the ST link updater my programmer suddenly not recognize the target board.

I tried to reflash with different versions but it says that is corrupted. Is the ST link updater the same for all the st link programmers?

Thank you!

This topic has been closed for replies.

3 replies

afla03Author
Associate
June 19, 2023

I actually have 2 other ST link V2 and the connections are exactly the same, I am able to program the boards with the other 2.

Pavel A.
June 19, 2023

Yes the st-link updater is one for all variants. Try the latest version, on a good computer (with *supported* Windows or Linux) and good cables.

Do not change other options (if shown): clock, mass storage drive, etc.

Peter BENSCH
ST Technical Moderator
June 25, 2023

If the problem still exists: Can you please upload a photo of the ST-LINK/V2 ISOL and mark the faulty one there?

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.