Skip to main content
GunkutA
Associate III
Jun 17, 2020 6:04 AM UTC
Solved

ST-Link V2, device not found error.

Hello. I just got a ST-Link V2 and wasn't able to program/debug a STM32 MCU with it. With a fake programmer I can program succesfully. But when I try to use ST-Link V2, it gives me device not found error. I wire STDIO, SWDCLK and GND pins to the target MCU and I power up the ST-Link v2 from USB connector. Do I also wire Reset pin or anyother pin? I started to think that the one I got was broken or something... Thanks before hand.

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jun 17, 2020 6:11 AM UTC

Pin 1 or 2 needs to be connected to the targets supply so the internal buffers are powered to the correct IO voltage.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jun 17, 2020 6:11 AM UTC

Pin 1 or 2 needs to be connected to the targets supply so the internal buffers are powered to the correct IO voltage.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
GunkutA
GunkutAAuthor
Associate III
Jun 17, 2020 6:12 AM UTC

Thank you