Skip to main content
MLemo.1
Associate III
Jun 26, 2020 6:37 PM UTC
Solved

ST-link V2 appears as a USB device instead of a COM PORT

Hello,

Like the title says when I connect an ST-link to a computer to try to program an NRF52 through an arduino with it it won't show up on COM port but can be found in device manager under "USB devices" as can seen by this picture:

 0693W000001rcrIQAQ.png

How do you fix that problem and make the device appear as a COM port?

BTW I have a similar problem with the original ST link and J link as well.

This topic has been closed for replies.

5 replies

Pavel A.
Jun 27, 2020 9:26 PM UTC

Does your ST-Link V2 have a VCOM function? If not - this is normal, not a problem.

The usual white ST-Link v2 dongles do not have VCOM. Bring your own USB to TTL UART adapter.

-- pa

MLemo.1
MLemo.1Author
Associate III
Jun 27, 2020 10:59 PM UTC

It used to show up as a com port an year ago but didn't touch it since then and not realy sure what happened I also remembering fidling with it's drivers a bit

Pavel A.
Jun 28, 2020 12:40 PM UTC

Please select the "STM32 STlink" in dev. manager, then click View-> Devices by container. Post the picture.

-- pa

MLemo.1
MLemo.1AuthorBest answer
Associate III
Jun 28, 2020 6:14 PM UTC