Question
ST-Link Utility : Mass flash erase fails, however erase bank 1 and 2 works
Posted on December 01, 2017 at 16:13
I can connect to my MCU with the ST-Link Utility and ST-Link V2. I can perform an erase of Bank 1 and Bank 2
(Target -> Erase Bank1). I can perform an erase of all flash pages (Target -> Erase Sectors...).
However, the st-link utility fails to perform a 'flash erase' (Target -> Erase Chip), I get the message 'Error occured during flash mass erase!'
I tried to perform a full flash erase with Keil UV5 with the same result: I get an error, however I am able to erase individual sectors or banks.
My setup:
MCU (STM32L476RGT6)
ST-Link Utility (v4.1.0.0)
ST-Link V2 (V2.J28.S7)
#stm32l476 #stm32l476-flash #st-link-utility #stm32-st-link-utility #flash-erase #st-link-utility