Skip to main content
JAlca
Associate III
January 28, 2020
Question

ST-LINK (Reason: (4) No device found on target.) custom board with STM32F303CCT6

  • January 28, 2020
  • 5 replies
  • 831 views

Hi all,

I have a custom board, with a STM32F303CCT6, but I cant to connect with ST-LINK.

For simplicity, I only soldered the MCU, the 4 capacitor on the power pins and the reset circuit. I tested with BOOT0 to GND and to VCC, but nothing works.

I tested the MCU connecting by serial and I did read/write correctly, but I cant to connect by SWD.

Any advices?

This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
January 28, 2020

Part's not running/functional.

Check level on NRST pin.

Make sure VDDA and VSSA are connected to supplies.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
January 28, 2020

External ST-LINK, make sure pin 1 or 2 are connected to supply for board.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
JAlca
JAlcaAuthor
Associate III
January 29, 2020

In order to simplify the circuit, will start with this minimum configuration?:

-4 capacitors between VDD/VSS VDDA/VSSA

-NRST to VCC

-Power by ST-LINK

-Connect SWDIO

-Connect SWCLK

Tesla DeLorean
Guru
January 29, 2020

NRST should not be driven, there should be an internal pull-up, you can either leave unconnected, or connect to SWD/JTAG header.

Check device orientation.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..