Skip to main content
LCE
Principal III
October 9, 2023
Solved

ST-Link on Nucleos: F7 vs H7 - Limitations?

Hello,

last year I designed a prototype pcb with a F767, for programming I used the Nucleo-F767's SWD interface (with some jumpers switched), that worked perfectly.

Now I need to re-design that board, but with a H723/H733, and I just checked the Nucleo-H723 I've been working with, and I see that the ST-Link part is completely different, mostly SWD connector layout, and no more options with jumpers.

For now I would like to keep using the Nucleo-F767 including connector layout, but are there any limitations concerning MCU type or anything else?
Specifically, can I program / flash / debug a H723 with a Nucleo-F767's ST-Link?

Thanks in advance!

This topic has been closed for replies.
Pavel A.
Pavel A.Best answer
October 9, 2023

Nucleo-H7's have ST-LINK version 3 and the "standard" mini 10-pin connector, and Nucleo F7 has ST-LINKv2. The SWD pins should be compatible. There is no good reason not to get a new ST-LINKv3 to debug your H723. This is much easier than hook a 2nd Nucleo and faster because v.3 has high-speed USB. New ST-Links v3 have 14-pin connector and cable, two extra pins on each side. The central 10 pins are same as on the 10-pin connector, two side pins are for the VCP.

3 replies

Pavel A.
Pavel A.Best answer
October 9, 2023

Nucleo-H7's have ST-LINK version 3 and the "standard" mini 10-pin connector, and Nucleo F7 has ST-LINKv2. The SWD pins should be compatible. There is no good reason not to get a new ST-LINKv3 to debug your H723. This is much easier than hook a 2nd Nucleo and faster because v.3 has high-speed USB. New ST-Links v3 have 14-pin connector and cable, two extra pins on each side. The central 10 pins are same as on the 10-pin connector, two side pins are for the VCP.

Tesla DeLorean
Guru
October 9, 2023

ST-LINK/V2 will work fine, just slower

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
LCE
LCEAuthor
Principal III
October 9, 2023

Thanks, guys!

So yeah, for production later on I should directly go for the 14-pin connector, including the VCP.