Skip to main content
evert2
Associate III
October 24, 2013
Question

ST-link_CLI.exe verify function is not working

Posted on October 24, 2013 at 10:30

When I run the CLI tool for programming including a verify, this is not working:

R:\Shared\Evertz\Automatic ST-link program>ST-LINK_CLI.exe -P ''SYGDR scripts/Boo

tloaderSTM32F0xx-v02.bin'' -V 0x08000000

STM32 ST-LINK CLI v1.4.0

STM32 ST-LINK Command Line Interface

Connected via SWD.

Device ID:0x440

Device family :STM32F05x

Flash Programming:

  File : SYGDR scripts/BootloaderSTM32F0xx-v02.bin

  Address : 0x00000000

[0x00000000]:Invalid address!

When I only do a program it works fine,

Does anyone has any idea what is going on?

#st-link-cli-verify
This topic has been closed for replies.

1 reply

Amel NASRI
ST Technical Moderator
October 24, 2013
Posted on October 24, 2013 at 12:07

Hi Evert,

Try to put the address before the ''-V'' option.

There is a newer version of ST-LINK CLI (v1.7.0) available with

http://www.st.com/web/en/catalog/tools/FM147/SC1887/PF258168

.

-Mayla-

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.