Skip to main content
MFail.11
Associate III
February 16, 2024
Question

ST-Link cannot more flash external Target

Hello,

Situation: I have a Nucleo WB55 board that is able to flash the internal SMT32 micro with the embedded ST-Link.

I want to use this Nucleo to flash a custom board with the embbedded ST-LINK, disconnecting the jumpers and connecting the lines properly to the custom board. This process fails because Cube programmer don't find the STM32 target. It finds st-link of course and I tried every mode, every clock frequency, everithing.

So this Nucleo can flash internal target but not external one!

Strange things: With the same Nucleo weeks ago I was able to flash external target, now I can't, something happened.

Connections and continuity is OK, custom board is ok (I can flash it with others Nucleo boards), cables are ok, lines are properly connected.

So what a mistery is this?

This topic has been closed for replies.

7 replies

TDK
February 16, 2024

There's not many components at play here. The ST-Link doesn't care what it connects to, so the issue is the wiring.

Recheck GND, SWDIO, SWCLK between the st-link and the target mcu, and only between those two. Ensure target mcu is powered. That's it, apart from some corner cases.

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
MFail.11
MFail.11Author
Associate III
February 19, 2024

That's not it. Cables are ok, If I use a different Nucleo board with same external target and cables, I can flash the target.

The internal target when Jumpers are installed is detected perfectly from Cube Programmer.

I never powered the target MCU, the st link provide supply to external board and it worked always.

So if cables are ok an continuity is ok, something else is still present.

A damage that prevent to use long wires could be?

AScha.3
Super User
February 19, 2024

So try with low data speed to connect , because long wires.

If you feel a post has answered your question, please click on " Best Answer ".
AScha.3
Super User
February 16, 2024

Just try to reconnect the onboard cpu and connect to it - to prove, you didnt damage something.

If you feel a post has answered your question, please click on " Best Answer ".