Associate II
May 14, 2018
Question
ST-LINK 4.2.0.0 Utility crashes when programming specific HEX file to H7 MCU
- 7 replies
- 1845 views
Posted on May 14, 2018 at 13:41
I am able to connect to the target:
14:35:49 : ST-LINK SN : 0674FF3836314B3457144034
14:35:49 : ST-LINK Firmware version : V2J29M18
14:35:49 : Connected via SWD.
14:35:49 : SWD Frequency = 4,0 MHz.
14:35:49 : Connection mode : Normal.
14:35:50 : Device ID:0x450
14:35:50 : Device flash Size : 2MBytes
14:35:50 : Device family :STM32H7xx
But when programming, it crashes with an error 'STM32 ST-LINK utility MFC Application has stopped working' and returned error code is equal to1073740940
.Please find hex file attached. It works when programming directly from KEIL using ST-link. Do you know what is going on here?
#hex #st-link-utility