Associate III
June 21, 2022
Question
Sram not working if writing in eprom with spi
- 6 replies
- 3737 views
Hi community..
I am working with mcu STM32F429 and SRAM with code IS42S16400J .
I have developed a code for init and working with this sram and it was working
void SDRAM_Init(void)
{
volatile uint32_t ptr = 0;
volatile uint32_t i = 0;
/* PB5,PB6 */
GPIOB -> MODER |= ((GPIOB -> MODER) & 0xFFFFC3FF ) | 0x00002800; // AF Function
GPIOB -> OTYPER |= ((GPIOB -> OTYPER) & 0xFFFFFF9F); // Push-Pull
GPIOB -> OSPEEDR |= ((GPIOB -> OSPEEDR) & 0xFFFFC3FF) | 0x00003C00; // Very High Speed
GPIOB -> PUPDR |= ((GPIOB -> PUPDR) & 0xFFFFC3FF); // No Pull-Up
GPIOB -> AFR[0] |= ((GPIOB -> AFR[0]) & 0xF00FFFFF) | 0x0CC00000; //
GPIOB -> AFR[1] |= ((GPIOB -> AFR[1]) & 0xFFFFFFFF) | 0x00000000; //
/* PC0 */
GPIOC -> MODER |= ((GPIOC -> MODER) & 0xFFFFFFFC) | 0x00000002; // AF Function
GPIOC -> OTYPER |= ((GPIOC -> OTYPER) & 0xFFFFFFFE); // Push-Pull
GPIOC -> OSPEEDR |= ((GPIOC -> OSPEEDR) & 0xFFFFFFFC) | 0x00000003; // Very High Speed
GPIOC -> PUPDR |= ((GPIOC -> PUPDR) & 0xFFFFFFFC); // No Pull-Up
GPIOC -> AFR[0] |= ((GPIOC -> AFR[0]) & 0xFFFFFFF0) | 0x0000000C; //
GPIOC -> AFR[1] |= ((GPIOC -> AFR[1]) & 0xFFFFFFFF) | 0x00000000; //
/* PD0,PD1,PD8,PD9,PD10,PD14,PD15 */
GPIOD -> MODER |= ((GPIOD -> MODER) & 0x0FC0FFF0) | 0xA02A000A; // AF Function
GPIOD -> OTYPER |= ((GPIOD -> OTYPER) & 0xFFFF38FC); // Push-Pull
GPIOD -> OSPEEDR |= ((GPIOD -> OSPEEDR) & 0x0FC0FFF0) | 0xF03F000F; // Very High Speed
GPIOD -> PUPDR |= ((GPIOD -> PUPDR) & 0x0FC0FFF0); // No Pull-Up
GPIOD -> AFR[0] |= ((GPIOD -> AFR[0]) & 0xFFFFFF00) | 0x000000CC; //
GPIOD -> AFR[1] |= ((GPIOD -> AFR[1]) & 0x00FFF000) | 0xCC000CCC; //
/* PE0,PE1,PE7,PE8,PE9,PE10,PE11,PE12,PE13,PE14,PE15 */
GPIOE -> MODER |= ((GPIOE -> MODER) & 0x00003FF0) | 0xAAAA800A; // AF Function
GPIOE -> OTYPER |= ((GPIOE -> OTYPER) & 0xFFFF007C); // Push-Pull
GPIOE -> OSPEEDR |= ((GPIOE -> OSPEEDR) & 0x00003FF0) | 0xFFFFC00F; // Very High Speed
GPIOE -> PUPDR |= ((GPIOE -> PUPDR) & 0x00003FF0); // No Pull-Up
GPIOE -> AFR[0] |= ((GPIOE -> AFR[0]) & 0x0FFFFF00) | 0xC00000CC; //
GPIOE -> AFR[1] |= ((GPIOE -> AFR[1]) & 0x00000000) | 0xCCCCCCCC; //
/* PF0,PF1,PF2,PF3,PF4,PF5,PF11,PF12,PF13,PF14,PF15 */
GPIOF -> MODER |= ((GPIOF -> MODER) & 0x003FF000) | 0xAA800AAA; // AF Function
GPIOF -> OTYPER |= ((GPIOF -> OTYPER) & 0xFFFF07C0); // Push-Pull
GPIOF -> OSPEEDR |= ((GPIOF -> OSPEEDR) & 0x003FF000) | 0xFFC00FFF; // Very High Speed
GPIOF -> PUPDR |= ((GPIOF -> PUPDR) & 0x003FF000); // No Pull-Up
GPIOF -> AFR[0] |= ((GPIOF -> AFR[0]) & 0xFF000000) | 0x00CCCCCC; //
GPIOF -> AFR[1] |= ((GPIOF -> AFR[1]) & 0x00000FFF) | 0xCCCCC000; //
/* PG0,PG1,PG4,PG5,PG8,PG15 */
GPIOG -> MODER |= ((GPIOG -> MODER) & 0x3FFCF0F0) | 0x80020A0A; // AF Function
GPIOG -> OTYPER |= ((GPIOG -> OTYPER) & 0xFFFF7ECC); // Push-Pull
GPIOG -> OSPEEDR |= ((GPIOG -> OSPEEDR) & 0x3FFCF0F0) | 0xC0030F0F; // Very High Speed
GPIOG -> PUPDR |= ((GPIOG -> PUPDR) & 0x3FFCF0F0); // No Pull-Up
GPIOG -> AFR[0] |= ((GPIOG -> AFR[0]) & 0xFF00FF00) | 0x00CC00CC; //
GPIOG -> AFR[1] |= ((GPIOG -> AFR[1]) & 0x0FFFFFF0) | 0xC000000C; //
RCC->AHB3ENR |= RCC_AHB3ENR_FMCEN;
// Initialization step 1
FMC_Bank5_6->SDCR[0] = FMC_SDCR1_SDCLK_1 | FMC_SDCR1_RBURST | FMC_SDCR1_RPIPE_1;
FMC_Bank5_6->SDCR[1] = FMC_SDCR1_NR_0 | FMC_SDCR1_MWID_0 | FMC_SDCR1_NB | FMC_SDCR1_CAS;
// Initialization step 2
FMC_Bank5_6->SDTR[0] = TRC(7) | TRP(2);
FMC_Bank5_6->SDTR[1] = TMRD(2) | TXSR(7) | TRAS(4) | TWR(2) | TRCD(2);
// Initialization step 3
while(FMC_Bank5_6->SDSR & FMC_SDSR_BUSY);
FMC_Bank5_6->SDCMR = 1 | FMC_SDCMR_CTB2 | (1 << 5);
// Initialization step 4
for(i = 0; i < 1000000; i++);
// Initialization step 5
while(FMC_Bank5_6->SDSR & FMC_SDSR_BUSY);
FMC_Bank5_6->SDCMR = 2 | FMC_SDCMR_CTB2 | (1 << 5);
// Initialization step 6
while(FMC_Bank5_6->SDSR & FMC_SDSR_BUSY);
FMC_Bank5_6->SDCMR = 3 | FMC_SDCMR_CTB2 | (4 << 5);
// Initialization step 7
while(FMC_Bank5_6->SDSR & FMC_SDSR_BUSY);
FMC_Bank5_6->SDCMR = 4 | FMC_SDCMR_CTB2 | (1 << 5) | (0x231 << 9);
// Initialization step 8
while(FMC_Bank5_6->SDSR & FMC_SDSR_BUSY);
FMC_Bank5_6->SDRTR |= (683 << 1);
while(FMC_Bank5_6->SDSR & FMC_SDSR_BUSY);
// Clear SDRAM
// for(ptr = SDRAM_BASE; ptr < (SDRAM_BASE + SDRAM_SIZE); ptr += 4)
// *((uint32_t *)ptr) = 0x07e007e0;
// for(ptr = SDRAM_BASE; ptr < (SDRAM_BASE + 959); ptr += 4)
// *((uint32_t *)ptr) = 0xFFFFFFFF;
for(ptr = SDRAM_BASE; ptr < (SDRAM_BASE + 0xc7ff); ptr += 4)
*((uint32_t *)ptr) = 0x07e007e0;
for(ptr = SDRAM_BASE + 0xc800; ptr < (SDRAM_BASE + 0x18fff); ptr += 4)
*((uint32_t *)ptr) = 0xf800f800;
for(ptr = SDRAM_BASE + 0x19000; ptr < (SDRAM_BASE + SDRAM_SIZE); ptr += 4)
*((uint32_t *)ptr) = 0x001f001f;
}Then we decided to use an external eeprom for saving some parameters using the following chip AT25640..
I developed the code in a separated project by using the HAL SPI for communicating and saving the parametrs and it was working.
/**
* @brief Function for writing the eeprom
* @param *spi2Handle
* @param *txBuffer
* @param size
* @param addr
* @retval EEPROM_ERROR or EEPROM_OK
*/
uint8_t WriteEEPROM(SPI_HandleTypeDef *spi2Handle, uint8_t *txBuffer, uint16_t size, uint16_t addr)
{
uint8_t addrLow = addr & 0xFF;
uint8_t addrHigh = (addr >> 8);
uint8_t wrenInstruction = WREN_EEPROM;
uint8_t buffer[32] = {WRITE_EEPROM, addrHigh, addrLow};
for(uint8_t i = 0 ; i < size ; i++)
{
buffer[3+i] = txBuffer[i];
}
/*chip select*/
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, RESET);
if(HAL_SPI_Transmit(spi2Handle, &wrenInstruction, 1, TIMEOUT_EEPROM) != HAL_OK)
{
return EEPROM_ERROR;;
}
/*chip select*/
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, SET);
/*delay in ms*/
HAL_Delay(10);
/*chip select*/
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, RESET);
if(HAL_SPI_Transmit(spi2Handle, buffer, (size + 3), TIMEOUT_EEPROM) != HAL_OK)
{
return EEPROM_ERROR;
}
/*delay in ms*/
HAL_Delay(10);
/*chip select*/
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, SET);
return EEPROM_OK;
}When I have imported this function within the project with the init of the sram the sram was not working anymore..
I really i don't understand why an init function is not working by calling the hal spi transmit for writing in eeprom ?
Any idea ?
Do you see something wrong in the init of the code of the sram?
Thanks a lot