Skip to main content
Archadious
Associate III
August 24, 2025
Solved

SPI on STM32G031

I'm attempting to configure SPI1 on an STM32G031.   However I must be missing something because there is no data being output.   I am trying setup SPI to transmit 16 bits at a time.  Any suggestions would be appreciated.   I'm running the uC at 64Mhz.

// Configure PA4 as the SPI select pin
//-----------------------------------------------------------------------------
void spi::nss( ) {

 GPIOA->MODER &= ~(GPIO_MODER_MODE4); // clear the mode bits for PA4
 GPIOA->MODER |= GPIO_MODER_MODE4_0; // Set PA4 as output mode
 GPIOA->OTYPER &= ~(GPIO_OTYPER_OT4); // Push-pull output on PA4
 GPIOA->OSPEEDR |= GPIO_OSPEEDR_OSPEED4; // Set PA4 for High Speed
 GPIOA->PUPDR &= ~(GPIO_PUPDR_PUPD4); // No pull-up/pull-down on PA4

}; // end css


// Configure pin PA5 as the SPI clock pin
//-----------------------------------------------------------------------------
void spi::sck( ) {

 GPIOA->MODER &= ~(GPIO_MODER_MODE5); // clear the mode bits for PA5
 GPIOA->MODER |= GPIO_MODER_MODE5_1; // Set PA5 to Alternate Function Mode
 GPIOA->OTYPER &= ~(GPIO_OTYPER_OT5); // Push-pull output on PA5
 GPIOA->OSPEEDR |= GPIO_OSPEEDR_OSPEED5; // Set speed of PA5 to Very High
 GPIOA->AFR[ 0 ] &= ~(GPIO_AFRL_AFSEL5); // Set PA5 Alt Function to SPI1_SCK

}; // end clock


// Configure pin PA7 as the SPI Master-Out-Slave-In pin
//-----------------------------------------------------------------------------
void spi::mosi( ) {

 GPIOA->MODER &= ~(GPIO_MODER_MODE7); // clear the mode bits for PA5
 GPIOA->MODER |= GPIO_MODER_MODE7_1; // Set PA7 to Alternate Function Mode
 GPIOA->OTYPER &= ~(GPIO_OTYPER_OT7); // Push-pull output on PA5
 GPIOA->OSPEEDR |= GPIO_OSPEEDR_OSPEED7; // Set speed of PA5 to Very High
 GPIOA->AFR[ 0 ] &= ~(GPIO_AFRL_AFSEL7); // Set PA7 Alt Function to SPI1_SCK

}; // end mosi


// Write 16 bits to SPI
//-----------------------------------------------------------------------------
void spi::write16( uint16_t data ) {

 printf( "spi::write16 data: %lx\r\n", data );

 select(); // NSS pin to low

 while( !( SPI1->SR & SPI_SR_TXE ) ) __NOP();
 *(volatile uint16_t*)&SPI1->DR = data;
 while( SPI1->SR & SPI_SR_BSY ) __NOP();

 deselect(); // NSS pin to high

}; // end write16


//-----------------------------------------------------------------------------
spi::spi( ) {

 printf( "spi::spi\r\n" );

 // Enable the RCC clocks for both GPIOA and SPI1
 RCC->IOPENR |= RCC_IOPENR_GPIOAEN; // enable the GPIOA clock
 RCC->APBENR2 |= RCC_APBENR2_SPI1EN; // enable the SPI1 clock

 // GPIO settings
 nss();
 sck();
 mosi();

 // Configure SPI1
 SPI1->CR1 &= SPI_CR1_SPE; // disable SPI1

 SPI1->CR1 = 0; // clear out the cr1 register
 SPI1->CR1 |= SPI_CR1_MSTR; // Master mode for SPI1

 SPI1->CR1 |= SPI_CR1_SSM | SPI_CR1_MSTR | SPI_CR1_SSI;
 SPI1->CR1 &= ~( SPI_CR1_CPOL | SPI_CR1_CPHA );
 SPI1->CR1 &= ~SPI_CR1_LSBFIRST; // MSB first

 SPI1->CR1 &= ~SPI_CR1_BR; // Clear BR bits
 SPI1->CR1 |= ( SPI_CR1_BR_2 | SPI_CR1_BR_0 ); // 101 -> /64


 SPI1->CR2 = 0; // clear cr2 register
 SPI1->CR2 |= SPI_CR2_DS; // Set 16-bit data
 SPI1->CR2 &= ~SPI_CR2_FRXTH; // RXNE set at 16-bits

 SPI1->CR1 |= SPI_CR1_SPE; // enable SPI1

}; // end spi
 

  

This topic has been closed for replies.
TDK
TDKBest answer
August 24, 2025

> SPI1->CR1 &= SPI_CR1_SPE; // disable SPI1

Missing a ~. Probably not the main issue.

> SPI1->CR2 = 0;

Can't set DS field to 0. Probably not the main issue.

 

> no data being output

Verified how?

If you set pins as GPIO output and toggle, can you see them toggle?

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
August 24, 2025

> SPI1->CR1 &= SPI_CR1_SPE; // disable SPI1

Missing a ~. Probably not the main issue.

> SPI1->CR2 = 0;

Can't set DS field to 0. Probably not the main issue.

 

> no data being output

Verified how?

If you set pins as GPIO output and toggle, can you see them toggle?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Archadious
Associate III
August 24, 2025

Thank you.  Your suggestions were invaluable!  

 

It's just what they say about another pair of eyes.  The issue was hardware related and staring me in the face for days.  I took your suggestion about toggling the pins as simple output.  Nothing.  So I rechecked all the hardware connections and ...  well, now I again feel foolish.  Thank you for your help.  

 

-A