Skip to main content
Associate III
July 16, 2024
Question

SPI Loopback test on stm32h563zit6

HI, STM Experts,

                Using STM32CubeIDE, I configured a project with default settings for the STM32H563ZIT6 (8 MHz external clock), running at 250 MHz. Additionally, I've enabled SPI1 for full duplex communication (transmitting and receiving simultaneously), with a data size of 8 bits, clock polarity (clk pol) = 0, clock phase (clk ph) = 1, and set the prescaler to 2, resulting in a baud rate of 125.0 Mbits/s. It's usually possible to wire MOSI to MISO. However, when I try to receive data from SPI1, it doesn't work. I don't know where I made a mistake. Could anyone please support me?

uint8_t tx_buffer[] = { 'H', 'e', 'l', 'l', 'o', '\r', '\n' };
uint8_t rx_buffer[20];

while (1)
 {
	 //HAL_UART_Transmit(&huart7, tx_buffer, sizeof(tx_buffer), 100);
 HAL_Delay(1000);
 for (int i = 0; i < sizeof(tx_buffer); i++)
 {
 HAL_SPI_TransmitReceive(&hspi1, tx_buffer + i, rx_buffer, 1, 100);
 HAL_UART_Transmit(&huart7, rx_buffer, sizeof(rx_buffer), 100);
 HAL_Delay(200);
 }
 }
static void MX_SPI1_Init(void)
{
 /* SPI1 parameter configuration*/
 hspi1.Instance = SPI1;
 hspi1.Init.Mode = SPI_MODE_MASTER;
 hspi1.Init.Direction = SPI_DIRECTION_2LINES;
 hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
 hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
 hspi1.Init.NSS = SPI_NSS_SOFT;
 hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
 hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi1.Init.CRCPolynomial = 0x7;
 hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
 hspi1.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
 hspi1.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
 hspi1.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
 hspi1.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
 hspi1.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
 hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
 hspi1.Init.IOSwap = SPI_IO_SWAP_DISABLE;
 hspi1.Init.ReadyMasterManagement = SPI_RDY_MASTER_MANAGEMENT_INTERNALLY;
 hspi1.Init.ReadyPolarity = SPI_RDY_POLARITY_HIGH;
 if (HAL_SPI_Init(&hspi1) != HAL_OK)
 {
 Error_Handler();
 }
}
This topic has been closed for replies.

14 replies

Associate III
July 16, 2024

sorry for my post its working good but i have an doubt

i am testing loop back test on spi1 on stm32h563zit6 microcontroller

hardware connection:

spi1:

mosi---------->miso

 

uint8_t tx_buffer[] = { 'H', 'e', 'l', 'l', 'o', '\r', '\n' };
uint8_t rx_buffer[20];
while (1)
{
     HAL_Delay(1000);
       HAL_SPI_TransmitReceive(&hspi1, tx_buffer , rx_buffer, sizeof(tx_buffer), 100);
       HAL_UART_Transmit(&huart7, rx_buffer, sizeof(rx_buffer), 100);
       HAL_Delay(200);
     }
   }

Whenever I use the HAL_SPI_TransmitReceive function, it works well. However, when I try to use HAL_SPI_Transmit and HAL_SPI_Receive  functions instead of HAL_SPI_TransmitReceive , it doesn't work. What could be the problem? How can I make it work?

 

while (1)

{

HAL_Delay(1000);

HAL_SPI_Transmit(&hspi1, tx_buffer, sizeof(tx_buffer), 100);

HAL_SPI_Receive(&hspi1, rx_buffer, sizeof(rx_buffer), 100);

HAL_UART_Transmit(&huart7, rx_buffer, sizeof(rx_buffer), 100);

HAL_Delay(200);

}

}

Mike_ST
ST Technical Moderator
July 16, 2024

Hello,

When you're calling HAL_SPI_Transmit(), the chip is not ready to receive anything, so it is transmitting in the void.

and when you're calling HAL_SPI_Receive(), nobody is sending anything, so time out occurs.

So, maybe call  HAL_SPI_Receive_IT (and prepare the SPI ISR) before transmitting so the chip is ready to receive the data.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Associate III
July 16, 2024

thank you @Mike_ST  any reference?

TDK
July 16, 2024
"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate III
July 16, 2024

@Mike_ST any reference code?

Associate II
July 16, 2024

I mean... people already gave you almost everything above.
As discussed in the topic shared by @TDK, the solution is the same.
Modify your CubeMX project to enable SPI interrupts.
Then run something like this:

bool rx_compltet = false;

int main(void)
{
 uint8_t tx_buffer[] = { 'H', 'e', 'l', 'l', 'o', '\r', '\n' };
 uint8_t rx_buffer[20];
 while (1)
 {
 HAL_Delay(1000);

 HAL_SPI_Receive_IT(&hspi1, rx_buffer, sizeof(rx_buffer), 100);

 HAL_SPI_Transmit(&hspi1, tx_buffer, sizeof(tx_buffer), 100);

 HAL_Delay(200);
 if(rx_complete == true)
 {
 HAL_UART_Transmit(&huart7, rx_buffer, sizeof(rx_buffer), 100);
 }
 }
}

void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
{
 if(hspi->Instance == SPI1)
 {
 rx_complete = true;
 }
}

 

Associate III
July 17, 2024

OK.. Thank you

Associate II
July 17, 2024

Did that helped?
Did you succeed with your loop back ?