Skip to main content
Associate
May 7, 2024
Question

Resetting the DFSDM Peripheral not working

I tried to reset the DFSDM1 Peripheral for two days using the STM32H7A3ZI and STM32Cube FW_H7 V1.11.1 (If that's important)

I want to Change OversamplingRatio and RightBitShift during the run of my program.

Apparently you do this by calling:

 

MX_DFSDM1_Init();

if(HAL_DFSDM_ChannelDeInit(&hdfsdm1_channel0) != HAL_OK){
Error_Handler();
}
if(HAL_DFSDM_ChannelDeInit(&hdfsdm1_channel1) != HAL_OK){
Error_Handler();
}
if(HAL_DFSDM_ChannelDeInit(&hdfsdm1_channel3) != HAL_OK){
Error_Handler();
}
if(HAL_DFSDM_FilterDeInit(&hdfsdm1_filter0) != HAL_OK){
Error_Handler();
}
if(HAL_DFSDM_FilterDeInit(&hdfsdm1_filter1) != HAL_OK){
Error_Handler();
}
if(HAL_DFSDM_FilterDeInit(&hdfsdm1_filter3) != HAL_OK){
Error_Handler();
}

__HAL_RCC_DFSDM1_CLK_ENABLE();
__HAL_RCC_DFSDM_FORCE_RESET();
__HAL_RCC_DFSDM_RELEASE_RESET();
__HAL_RCC_DFSDM1_CLK_ENABLE();

MX_DFSDM1_Init();

 

I tried to experiment with the CLK_ENABLE(); because another Post mentioned a possible Bug in 2021.

Without resetting and Deinit/Reinit my DFSDM with DMA works normally and it writes to the array, i start the DFSDM using this:

 

 

HAL_DFSDM_FilterRegularMsbStart_DMA(&hdfsdm1_filter0, getMainStorageCH1(), 40000);
HAL_DFSDM_FilterRegularMsbStart_DMA(&hdfsdm1_filter1, getMainStorageCH2(), 40000);
HAL_DFSDM_FilterRegularMsbStart_DMA(&hdfsdm1_filter3, getMainStorageCH3(), 40000);

 

the get Function return int16_t* to the Array. I use Oversampling of 512 and RightBitShift of 4

(but it shouldn't matter). No Error occurs when re-initializing, but the DFSDM doesn't write the Array

and doesn't fire ConversionHalf/Full Interrupts. I made Screenshots of the registers:

Channel 0 Without ResettingChannel 0 Without ResettingChannel 0 After ResettingChannel 0 After ResettingFilter 1 Without ResettingFilter 1 Without ResettingFilter 1 After ResettingFilter 1 After Resetting

 

Caption describes what was before and after Reset. I see a difference in some Registers but i dont want to spend days again learning the registers and how they work. Does anyone have a solution or is there another way to change Oversampling Ratio and Right Bit Shift without restarting the controller?

 

 

 

This topic has been closed for replies.

2 replies

Visitor II
July 3, 2024

Hi, I have the same problem on STM32L476. I tried to reset the DFSDM module in RCC but no success. Once I clear the DFEN bit the module stops working.

 

Associate II
July 3, 2024

This could be caused by the shared clock being initialized/deinitialized by these functions.
Like mentioned in this post.

 

You could try to add something like this:

if(DFSDM1_Init != 0) // Make sure to not execute DFSDM1_Init--; if == 0 (=0xFFFF FFFF)
{
 DFSDM1_Init-- ;
}

 

In your functions HAL_DFSDM_FilterMspDeInit and HAL_DFSDM_ChannelMspDeInit:

void HAL_DFSDM_FilterMspDeInit(DFSDM_Filter_HandleTypeDef* dfsdm_filterHandle)
{
 if(DFSDM1_Init != 0) // Make sure to not execute DFSDM1_Init--; if == 0 (=0xFFFF FFFF)
 {
 DFSDM1_Init-- ;
 }
 if(DFSDM1_Init == 0)
 {
 /* USER CODE BEGIN DFSDM1_MspDeInit 0 */

 /* USER CODE END DFSDM1_MspDeInit 0 */
 /* Peripheral clock disable */
 __HAL_RCC_DFSDM1_CLK_DISABLE();

 /**DFSDM1 GPIO Configuration
 PD6 ------> DFSDM1_DATIN1
 PD3 ------> DFSDM1_CKOUT
 PE4 ------> DFSDM1_DATIN3
 PD7 ------> DFSDM1_DATIN4
 */
 HAL_GPIO_DeInit(GPIOD, GPIO_PIN_6|GPIO_PIN_3|GPIO_PIN_7);

 HAL_GPIO_DeInit(GPIOE, GPIO_PIN_4);

 /* DFSDM1 DMA DeInit */
 HAL_DMA_DeInit(dfsdm_filterHandle->hdmaInj);
 HAL_DMA_DeInit(dfsdm_filterHandle->hdmaReg);

 /* USER CODE BEGIN DFSDM1_MspDeInit 1 */

 /* USER CODE END DFSDM1_MspDeInit 1 */
 }
}

void HAL_DFSDM_ChannelMspDeInit(DFSDM_Channel_HandleTypeDef* dfsdm_channelHandle)
{
 if(DFSDM1_Init != 0) // Same verification here !
 {
 DFSDM1_Init-- ;
 }
 if(DFSDM1_Init == 0)
 {
 /* USER CODE BEGIN DFSDM1_MspDeInit 0 */

 /* USER CODE END DFSDM1_MspDeInit 0 */
 /* Peripheral clock disable */
 __HAL_RCC_DFSDM1_CLK_DISABLE();

 /**DFSDM1 GPIO Configuration
 PD6 ------> DFSDM1_DATIN1
 PD3 ------> DFSDM1_CKOUT
 PE4 ------> DFSDM1_DATIN3
 PD7 ------> DFSDM1_DATIN4
 */
 HAL_GPIO_DeInit(GPIOD, GPIO_PIN_6|GPIO_PIN_3|GPIO_PIN_7);

 HAL_GPIO_DeInit(GPIOE, GPIO_PIN_4);

 /* USER CODE BEGIN DFSDM1_MspDeInit 1 */

 /* USER CODE END DFSDM1_MspDeInit 1 */
 }
}

 

This should avoid init/deinit clock conflicts.

 

Hope that will help.

Sulian