Skip to main content
Gpeti
Senior
September 5, 2022
Question

Remotely resetting a STM32H7 eval board

I want to remotely reset and start a STM32H753 eval board.

The board is connected to a PC through STLink and on this PC I run STLink-gdb-server in persistent mode.

ST-LINK_gdbserver.exe -d -e -v -p 61234 -a 400000000 -b 200 -i *** -cp "***"

On my development PC, I want to use gdb to reset the target, start execution.

The following works except that if I execute the command a second time, it terminates the gdbserver executable.

$(GDB) -q -ex "set confirm off" -ex "target extended-remote ***:61234" -ex "monitor reset halt" -ex "detach" -ex "quit"

According to gdb user manual, the detach command should not terminate gdbserver in "extended-remote" mode.

i tried several variations of the gdb command line but none of them is working.

Any idea ?

This topic has been closed for replies.

2 replies

mattias norlander
ST Employee
September 6, 2022

Hi,

We are able to re-produce the behavior on our machines, not necessarily the second time, but certainly reproducible.

extended-remote is not likely associated with this problem. Debug on-going on our side...

As a work-around you could launch the ST-LINK GDB-server from a bat-file which re-launches it as soon as the GDB-client has completed your debug command:

:loop
ST-LINK_gdbserver.exe -d -v -p 61234 -a 400000000 -b 200 -i *** -cp "***"
goto loop

Please notice "-e" (persistent mode) is removed from above suggested work-around since we rely on a loop instead...

Internal ticket reference: 134147

Gpeti
GpetiAuthor
Senior
September 7, 2022

hello,

Looping on gdbserver is not working. I think this is because it starts a new gdbserver after the target has been reset and started, so my guess is that the new gdbserver stops the execution on the target.