Skip to main content
MSimo.1
Associate III
October 28, 2020
Question

programm a L432 with a external vut-off STLink

Hey there,

i recently designed a PCB with a litte STM32 Procect.

Now i cant programm my MCU by SWD.

MCU : STM32L432KC

ST-Link : ST-Link v2.1 broken off a nucleo64 (according to UM1724)

ive got wires to pin 23 (SWDIO), pin 24 (SWCLK), pin 4 (NRST),GND and VCC of the MCU of my PCB.

i connected theese to CN4 of my ST-Link according to table 5 in UM1724.

i removed the 2 Jumpers on CN2 according to Table 4.

i connected VCC, GND (stlink+ my pcb) to external 3.3V from my power supply.

Then i created a new cubeIDE project and added an uint8_t wich increments every second. I selected Debug Serial Wire in SYS in the .ioc and tried to upload the code and got the following error:

STMicroelectronics ST-LINK GDB server. Version 5.5.0
Copyright (c) 2019, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
 Persistent Mode : Disabled
 Logging Level : 1
 Listen Port Number : 61234
 Status Refresh Delay : 15s
 Verbose Mode : Disabled
 SWD Debug : Enabled
 InitWhile : Enabled
 
Waiting for debugger connection...
Debugger connected
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.4.0 
 -------------------------------------------------------------------
 
ST-LINK SN : 066BFF575051717867092622
ST-LINK FW : V2J36M26
Voltage : 5.95V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x435
Device name : STM32L43xxx/STM32L44xxx
Flash size : 256 KBytes
Device type : MCU
Device CPU : Cortex-M4
 
 
 
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a01232.srec
 File : ST-LINK_GDB_server_a01232.srec
 Size : 11468 Bytes
 Address : 0x08000000 
 
 
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 5]
Download in Progress:
 
 
Error: failed to download Segment[0]
Error: failed to download the File
Encountered Error when opening F:\Programme\STM32CubeIDE_1.3.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.3.0.202002181050\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
 
Error in final launch sequence:
 
Failed to execute MI command:
load F:\\Programmieren\\STM32\\L432_SWDTest\\Debug\\L432_SWDTest.elf 
 
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load F:\\Programmieren\\STM32\\L432_SWDTest\\Debug\\L432_SWDTest.elf 
 
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load F:\\Programmieren\\STM32\\L432_SWDTest\\Debug\\L432_SWDTest.elf 
 
Error message from debugger back end:
Error finishing flash operation
Error finishing flash operation

any suggestions ?

do i have to change someting in the clock config in the .ioc? ive connected a 32khz XTAL between pin 2 and 3 of the L432. (this one : https://www.mouser.de/ProductDetail/NDK/NX3215SA-32768K-STD-MUA-8?qs=55YtniHzbhBdnrw6egvs7Q==)

This topic has been closed for replies.

2 replies

Peter BENSCH
ST Technical Moderator
October 29, 2020

All connections are fine, as you already get the correct Device ID of 0x435, the issue seems to have some other reason.

BTW: the two jumpers at CN2 cut the SWD connection to the target when the ST-LINK/V2-1 is still part of the NUCLEO. Their presence doesn't matter if you cut the ST-LINK to use it externally.

Do you use any low power mode of the L432 while trying to get connection?

But before we get into the details please update the tools as you are still using CubeIDE 1.3.0.

When your question is answered, please close this topic by choosing Select as Best.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
October 29, 2020
  1. Voltage : 5.95V

That's NOT good.

Connect the GND in common, no need to connect the VDD, the NUCLEO doesn't have buffers.

Try using the STM32 Cube Programmer

Make sure you don't have secondary devices/logic driving the NRST pin

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..