Skip to main content
Associate
September 18, 2023
Question

Problems starting debug of F439ZI

Hi,

 

I sometimes get this error when starting a Debug on an F439ZI

Error in final launch sequence:

 

Failed to start GDB server

Failed to start GDB server

Error in initializing ST-LINK device.

Reason: (5) Unknown MCU found on target.

 

Unplugging and replugging the USB to the ST-link fixes it, but it is a bit perplexing. Is there a better way?

This topic has been closed for replies.

3 replies

Issamos
Super User
September 18, 2023

Hello @alanb 

I think that the problem come from the port usb in your PC or the cable you are using.

I suggest you to try to change them.

Best regards.

II

TDK
September 20, 2023

Going into low power modes or changing the function of SWDIO/SWCLK pins can cause debugger connection issues.

Are you using a counterfeit programmer? Is this a custom board?

"If you feel a post has answered your question, please click ""Accept as Solution""."
alanbAuthor
Associate
October 13, 2023

No, I'm using a genuine Nucleo F439ZI board. But it was connected and powered from a laptop so it is I guess possible that the laptop USB didn't supply enough current. I have added an external power connector to my daughterboard.