Skip to main content
DBrau.2
Associate III
Nov 18, 2020 6:32 PM UTC
Solved

Problem with connection STM32H745

I've made a mistake and programmed to STM32h745 dual core processor program which was created to STM32H743 with one core. Now I have a problem with connection and ST-Link doesn't recognize device. What can I do with that?

I've also tried to supply board under reset (NRST pulled down to GND) and I get the fail "The interface firmware FAILED to reset/halt the target MCU".

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Nov 18, 2020 7:34 PM UTC

https://community.st.com/s/question/0D50X0000BRZL5NSQX/nucleoh745-stlink-utility-can-not-connect-to-target

Going to need to strap BOOT0 HIGH, and POWER CYCLE the board several times, until you can connect and delete your code.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

4 replies

Uwe Bonnes
Chief
Nov 18, 2020 6:42 PM UTC

You should leave the STLINK to handle the NRST line. Check only the box in Stm32CubeProg.

DBrau.2
DBrau.2Author
Associate III
Nov 18, 2020 6:59 PM UTC

In STM32CubeProg problem is exactly the same. No connection to the target

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Nov 18, 2020 7:34 PM UTC

https://community.st.com/s/question/0D50X0000BRZL5NSQX/nucleoh745-stlink-utility-can-not-connect-to-target

Going to need to strap BOOT0 HIGH, and POWER CYCLE the board several times, until you can connect and delete your code.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
DBrau.2
DBrau.2Author
Associate III
Nov 18, 2020 7:50 PM UTC

Thank you a lot. That was what I was looking for. Now the STM32 connects normally