Skip to main content
Associate
Aug 24, 2026 4:15 AM UTC
Question

POWERING UP STM32 NUCLEO L011K4

hi i have a  STM32 NUCLEO L011K4 working perfectly, i’m looking for ways where if i could power it up from external power source example battery through pins

 

3 replies

Senior III
Aug 24, 2026 4:42 AM UTC

Yes, the NUCLEO-L011K4 can be powered through its header pins:

  • For a 7-12 V battery/source, connect positive to Vin and negative to GND. The onboard regulator will generate the required voltages.
  • For a regulated 5 V source, connect it to the +5V pin and GND. Keep it within approximately 4.75-5.25 V.
  • A single 3.7 V Li-ion/LiPo battery cannot reliably power Vin; use a 5 V boost converter instead.
  • Avoid powering it simultaneously from USB and an external source. If USB is needed for debugging, apply external power first and then connect USB.

Direct 3.3 V injection is possible, but it bypasses the regulator and requires board solder-bridge changes, so I would avoid it unless you follow the Nucleo-32 manual carefully.

This STM32 board-design tutorial also provides a useful explanation of regulating an external 5 V source down to the 3.3 V required by an STM32.

rilsoAuthor
Associate
Aug 24, 2026 3:22 PM UTC

i tried supplying 5v using a regulator and then when check for the V on 5V and GND, i received 1.27v-1.37v

Same goes for 7-12v , source power of 8v to VIN, and GND, it receive 2.28V is this normal?
 or could there be an issue with the board/power path? Also, should I be measuring the voltage on some other pins?

Also what is the best way to indicate if the stm32 is receiving power and working properly?

Thanks

Mike_ST
ST Technical Moderator
Aug 31, 2026 8:38 AM UTC

Hello,

Please have a look at the documentation of the board (section 7.4 Power supply and power selection):

https://www.st.com/resource/en/user_manual/um1956-stm32-nucleo32-boards-mb1180-stmicroelectronics.pdf

 

And the schematic here:

https://www.st.com/resource/en/schematic_pack/nucleo-32pins_sch.zip

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.