Skip to main content
MRoss.21
Associate
December 29, 2020
Question

Power Supply Nucleo-F303K8

Hi! I have checked on Nucleo-F303K8's documentation that the required external power supply can be in a range of 3-3.6V. But what rechargeable LiPo battery can I use for this scope? I only found 3.7V ones!

This topic has been closed for replies.

1 reply

TDK
December 29, 2020

The voltage of a battery is a function of the battery chemistry. It's not something that can be chosen at will. For LiPo batteries, voltage is around 4.2V when fully charged, which is too high to use as the raw voltage necessary for the device.

You could connect the LiPo to the +5V input and it will work for most of the batteries life. This voltage passes through a LDO which will drop about 200mV.

"If you feel a post has answered your question, please click ""Accept as Solution""."