Question
Power Nucleo board directly from a single cell LiPo or Li-Ion
Posted on May 03, 2016 at 16:35
Is it possible to feed only the MCU on top of a Nucleo board without powering also the embedded ST-Link? I tried, but unfortunately the only solution seems to manually remove the connection between the ST-Link and the MCU reset line (plus removing the power line to the ST-Link). I would propose a more simple configuration, maybe adding an easily operable jumper like the EXT5V or USB5V selector. If anyone knows a simplier way, please let me know
#st-link #nucleo #hardware #swd