Skip to main content
BWate.1
Associate
Nov 11, 2020 9:02 AM UTC
Solved

Pin 1 and 2 on STDC14 of STLINK-V3SET

Is it ok to connect boot0 from STM32 (with a 10k pulldown to GND) to one of pin 1 or 2 on STDC14 from STLINK-V3SET?

The pins are 'reserved' regarding to the STLINK-V3SET manual p. 23 with the comment 'Do not connect on target' ;)

The boot0 should be ignored in this case, but we need boot0 for an alternative device.

Thanks!

This topic has been closed for replies.
Uwe Bonnes
Uwe BonnesBest answer
Chief
Nov 11, 2020 3:03 PM UTC

Actually PA7 is the SWD direction signal. PA7 high means SWD write, low means read.

4 replies

Uwe Bonnes
Chief
Nov 11, 2020 10:03 AM UTC

I checked on a V3 MOD board. There are internal connections on Pin 1/2 and, not like the for the other STDC14 pins, (obvious) 0-Ohm jumpers to isolate. So I would take the advice serious.

Uwe Bonnes
Chief
Nov 11, 2020 10:36 AM UTC
BWate.1
BWate.1Author
Associate
Nov 11, 2020 2:19 PM UTC

Thank you for the information.

Yes, I also think to connect something else isn't good...

BTW: Without a connection I have measured on the STDC14 from the STLINK-V3SET:

Pin 1: 5 V

Pin 2: 3,3 V

Uwe Bonnes
Uwe BonnesBest answer
Chief
Nov 11, 2020 3:03 PM UTC

Actually PA7 is the SWD direction signal. PA7 high means SWD write, low means read.