Skip to main content
BMäme.1
Associate II
March 9, 2022
Solved

OpenOCD crashes when starting from Windows Server 2016

Hi,

I tried to run OpenOCD on a virtual machine with Windows Server 2016. We using the version 1.3.0 of the STM32CubeIDE.

When I launch the OpenOCD the program crahses with the error message:

0693W00000Kbu2qQAB.pngOpenOCD is launched via this command:

CALL %PATH_STLink-OPENOCD%\openocd.exe -f %CD%\ReactionWheelTestFramework_Develop_Master.cfg -s %PATH_SUPPORTFILES% -d4

The debug log prints no error and ends like this

Info : 282 1797 core.c:1394 adapter_init(): clock speed 8000 kHz
Debug: 283 1797 openocd.c:142 handle_init_command(): Debug Adapter init complete
Debug: 284 1797 command.c:143 script_debug(): command - ocd_command ocd_command type ocd_transport init
Debug: 285 1813 command.c:143 script_debug(): command - ocd_transport ocd_transport init
Debug: 288 1813 transport.c:239 handle_transport_init(): handle_transport_init
Debug: 289 1813 hla_transport.c:152 hl_transport_init(): hl_transport_init
Debug: 290 1813 hla_transport.c:169 hl_transport_init(): current transport hla_swd
Debug: 291 1828 hla_interface.c:42 hl_interface_open(): hl_interface_open
Debug: 292 1828 hla_layout.c:40 hl_layout_open(): hl_layout_open
Debug: 293 1828 stlink_usb.c:2674 stlink_usb_open(): stlink_usb_open
Debug: 294 1828 stlink_usb.c:2688 stlink_usb_open(): transport: 1 vid: 0x0483 pid: 0x3744 serial:
Debug: 295 1844 stlink_usb.c:2688 stlink_usb_open(): transport: 1 vid: 0x0483 pid: 0x3748 serial:
Debug: 296 1844 stlink_usb.c:2688 stlink_usb_open(): transport: 1 vid: 0x0483 pid: 0x374b serial:
Debug: 297 1844 stlink_usb.c:2688 stlink_usb_open(): transport: 1 vid: 0x0483 pid: 0x374d serial:
Debug: 298 1860 stlink_usb.c:2688 stlink_usb_open(): transport: 1 vid: 0x0483 pid: 0x374e serial:
Debug: 299 1860 stlink_usb.c:2688 stlink_usb_open(): transport: 1 vid: 0x0483 pid: 0x374f serial:
Debug: 300 1860 stlink_usb.c:2688 stlink_usb_open(): transport: 1 vid: 0x0483 pid: 0x3752 serial:
Debug: 301 1875 stlink_usb.c:2688 stlink_usb_open(): transport: 1 vid: 0x0483 pid: 0x3753 serial:

Can someone help me? :)

Kind regards

Bastian

This topic has been closed for replies.
BMäme.1
BMäme.1Best answer
Associate II
March 10, 2022

Hi there,

thank you for your support.

I have solved this issure by updating the UTN-Server. Now i runs fine :)

Best regards

5 replies

LaurentL
ST Employee
March 9, 2022

Hello,

STM32CubeIde v1.3.0 is quite old.

v1.9.0 is out, update and tell us if you still have the issue.

Maybe linked to the STLink USB drivers ?

Did you install them ?

You have admin rights ?

Can the STLink debug works in STM32CubeIde (using Openocd debug server) ?

Rgds,

Laurent

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AntonioST
ST Employee
March 9, 2022

It looks like this known problem of OpenOCD with the new libusb 1.0.25

https://sourceforge.net/p/openocd/tickets/308/

https://sourceforge.net/p/openocd/tickets/336/

It has been fixed in upstream OpenOCD

http://review.openocd.org/6331/

but there is still no official OpenOCD release that includes it.

BMäme.1
BMäme.1Author
Associate II
March 9, 2022

Hello,

thank you for your help. :)

I have tried with version 1.8.0, there i have the same problem.

Yes, the STLink USB drivers are installed. I also have admin rights. The Nucleo board is connected via an UTN-Server (SEH myUTN 250).

It works fineOn my local PC :\

I also tried to launch the Openocd debug server via the STM32CubeIDE with version 1.3.0 and 1.8.0.

BMäme.1
BMäme.1Author
Associate II
March 9, 2022

I insert the libusb 1.0.25. Now I didn't get the error message of "openoced.exe has stopped working".

But the debug output gives me now an error:

Info : 282 1765 core.c:1394 adapter_init(): clock speed 8000 kHz
Debug: 283 1765 openocd.c:142 handle_init_command(): Debug Adapter init complete
Debug: 284 1781 command.c:143 script_debug(): command - ocd_command ocd_command type ocd_transport init
Debug: 285 1781 command.c:143 script_debug(): command - ocd_transport ocd_transport init
Debug: 288 1781 transport.c:239 handle_transport_init(): handle_transport_init
Debug: 289 1797 hla_transport.c:152 hl_transport_init(): hl_transport_init
Debug: 290 1797 hla_transport.c:169 hl_transport_init(): current transport hla_swd
Debug: 291 1797 hla_interface.c:42 hl_interface_open(): hl_interface_open
Debug: 292 1797 hla_layout.c:40 hl_layout_open(): hl_layout_open
Debug: 293 1812 stlink_usb.c:2674 stlink_usb_open(): stlink_usb_open
Debug: 294 1812 stlink_usb.c:2688 stlink_usb_open(): transport: 1 vid: 0x0483 pid: 0x3744 serial:
Debug: 295 1812 stlink_usb.c:2688 stlink_usb_open(): transport: 1 vid: 0x0483 pid: 0x3748 serial:
Debug: 296 1812 stlink_usb.c:2688 stlink_usb_open(): transport: 1 vid: 0x0483 pid: 0x374b serial:
Debug: 297 1828 stlink_usb.c:2688 stlink_usb_open(): transport: 1 vid: 0x0483 pid: 0x374d serial:
Debug: 298 1828 stlink_usb.c:2688 stlink_usb_open(): transport: 1 vid: 0x0483 pid: 0x374e serial:
Debug: 299 1828 stlink_usb.c:2688 stlink_usb_open(): transport: 1 vid: 0x0483 pid: 0x374f serial:
Debug: 300 1843 stlink_usb.c:2688 stlink_usb_open(): transport: 1 vid: 0x0483 pid: 0x3752 serial:
Debug: 301 1843 stlink_usb.c:2688 stlink_usb_open(): transport: 1 vid: 0x0483 pid: 0x3753 serial:
Error: 302 1859 stlink_usb.c:2702 stlink_usb_open(): open failed
Debug: 303 1859 hla_layout.c:47 hl_layout_open(): failed
Debug: 304 1859 command.c:642 run_command(): Command failed with error code -4
User : 305 1875 command.c:705 command_run_line():
Debug: 306 1875 command.c:642 run_command(): Command failed with error code -4
User : 307 1875 command.c:705 command_run_line():
Debug: 308 1875 target.c:2048 target_free_all_working_areas_restore(): freeing all working areas
Debug: 309 1890 hla_interface.c:117 hl_interface_quit(): hl_interface_quit

BMäme.1
BMäme.1AuthorBest answer
Associate II
March 10, 2022

Hi there,

thank you for your support.

I have solved this issure by updating the UTN-Server. Now i runs fine :)

Best regards