Skip to main content
usafape
Associate II
August 28, 2012
Question

OpenOCD and stlink-v2

Posted on August 28, 2012 at 09:03

I am trying to get OpenOCD to work with my STM32F4Discovery board and I get the following error:

fabio@fs-1:~/workspace/stm32_code/test$ openocd -d 3 -f ./openocd.cfg
Open On-Chip Debugger 0.6.0-rc1-dev-00015-g47728f9 (2012-08-27-23:46)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.sourceforge.net/doc/doxygen/bugs.html
User : 11 2 command.c:549 command_print(): debug_level: 3
Debug: 12 2 configuration.c:45 add_script_search_dir(): adding /home/fabio/.openocd
Debug: 13 2 configuration.c:45 add_script_search_dir(): adding /usr/local/share/openocd/site
Debug: 14 2 configuration.c:45 add_script_search_dir(): adding /usr/local/share/openocd/scripts
Debug: 15 2 configuration.c:86 find_file(): found ./openocd.cfg
Debug: 16 2 command.c:145 script_debug(): command - ocd_command ocd_command type ocd_telnet_port 4444
Debug: 17 2 command.c:145 script_debug(): command - telnet_port ocd_telnet_port 4444
Debug: 19 2 command.c:145 script_debug(): command - ocd_command ocd_command type ocd_gdb_port 3333
Debug: 20 2 command.c:145 script_debug(): command - gdb_port ocd_gdb_port 3333
Debug: 22 2 command.c:145 script_debug(): command - ocd_command ocd_command type ocd_interface stlink-v2
Debug: 23 2 command.c:145 script_debug(): command - interface ocd_interface stlink-v2
Error: 25 2 adapter.c:183 handle_interface_command(): The specified debug interface was not found (stlink-v2)
User : 26 2 command.c:549 command_print(): The following debug interfaces are available:
Debug: 27 2 command.c:631 run_command(): Command failed with error code -101
User : 28 2 command.c:669 command_run_line(): Runtime Error: ./openocd.cfg:5: 
in procedure 'script' 
at file ''embedded:startup.tcl'', line 58
in procedure 'interface' called at file ''./openocd.cfg'', line 5

I am using the following config file:

#daemon configuration
telnet_port 4444
gdb_port 3333
# Interface (using versaloon)
interface stlink-v2
transport select swd
swd_mode 2
swd_delay 2
set WORKAREASIZE 0x800
source [find target/stmcfg]

Can somebody shine me some light to this? #openocd-stlink
This topic has been closed for replies.

4 replies

andyturk
Associate II
August 28, 2012
Posted on August 28, 2012 at 19:31

This is just a guess, but maybe your openocd binary was compiled without the ''stlink-v2'' interface. Did you include ''--enable-stlink'' on the command line for configure?

Here's what I use:

./configure --verbose --enable-maintainer-mode --enable-stlink --no-create --no-recursion --disable-verbose-usb-io --disable-verbose-usb-comms

You can check the config.log file in your build directory to see how things are set up.

usafape
usafapeAuthor
Associate II
August 29, 2012
Posted on August 29, 2012 at 16:22

I've tried... no luck.

I am looking at the config.log file and there are errors. Here are the first few lines of it:

running configure, to aid debugging if configure makes a mistake.

It was created by openocd configure 0.6.0-rc1-dev, which was
generated by GNU Autoconf 2. Invocation command line was

 $ ./configure --verbose --enable-maintainer-mode --enable-stlink --no-create --no-recursion --disable-verbose-usb-io --disable-verbose-usb-comms

## --------- ##
## Platform. ##
## --------- ##

hostname = fs-1
uname -m = i686
uname -r = 3.2.0-29-generic-pae
uname -s = Linux
uname -v = #46-Ubuntu SMP Fri Jul 27 17:25:43 UTC 2012

/usr/bin/uname -p = unknown
/bin/uname -X = unknown

/bin/arch = unknown
/usr/bin/arch -k = unknown
/usr/convex/getsysinfo = unknown
/usr/bin/hostinfo = unknown
/bin/machine = unknown
/usr/bin/oslevel = unknown
/bin/universe = unknown

PATH: /usr/lib/lightdm/lightdm
PATH: /usr/local/sbin
PATH: /usr/local/bin
PATH: /usr/sbin
PATH: /usr/bin
PATH: /sbin
PATH: /bin
PATH: /usr/games
PATH: /home/fabio/sat/bin/
PATH: /home/fabio/apps/bin/
PATH: /home/fabio/sat/bin/


## ----------- ##
## Core tests. ##
## ----------- ##

configure:2515: checking for a BSD-compatible install
configure:2583: result: /usr/bin/install -c
configure:2594: checking whether build environment is sane
configure:2644: result: yes
configure:2785: checking for a thread-safe mkdir -p
configure:2824: result: /bin/mkdir -p
configure:2837: checking for gawk
configure:2867: result: no
configure:2837: checking for mawk
configure:2853: found /usr/bin/mawk
configure:2864: result: mawk
configure:2875: checking whether make sets $(MAKE)
configure:2897: result: yes
configure:2978: checking whether to enable maintainer-specific portions of Makefiles
configure:2987: result: yes
configure:3059: checking for gcc
configure:3075: found /usr/bin/gcc
configure:3086: result: gcc
configure:3315: checking for C compiler version
configure:3324: gcc --version >&5
gcc (Ubuntu/Linaro 4.6.3-1ubuntu5) 4.6.3
Copyright (C) 2011 Free Software Foundation, Inc.
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

configure:3335: $? = 0
configure:3324: gcc -v >&5
Using built-in specs.
COLLECT_GCC=gcc
COLLECT_LTO_WRAPPER=/usr/lib/gcc/i686-linux-gnu/4.6/lto-wrapper
Target: i686-linux-gnu
Configured with: ../src/configure -v --with-pkgversion='Ubuntu/Linaro 4.6.3-1ubuntu5' --with-bugurl=file:///usr/share/doc/gcc-4.6/README.Bugs --enable-languages=c,c++,fortran,objc,obj-c++ --prefix=/usr --program-suffix=-4.6 --enable-shared --enable-linker-build-id --with-system-zlib --libexecdir=/usr/lib --without-included-gettext --enable-threads=posix --with-gxx-include-dir=/usr/include/c++/4.6 --libdir=/usr/lib --enable-nls --with-sysroot=/ --enable-clocale=gnu --enable-libstdcxx-debug --enable-libstdcxx-time=yes --enable-gnu-unique-object --enable-plugin --enable-objc-gc --enable-targets=all --disable-werror --with-arch-32=i686 --with-tune=generic --enable-checking=release --build=i686-linux-gnu --host=i686-linux-gnu --target=i686-linux-gnu
Thread model: posix
gcc version 4.6.3 (Ubuntu/Linaro 4.6.3-1ubuntu5)
configure:3335: $? = 0
configure:3324: gcc -V >&5
gcc: error: unrecognized option '-V'
gcc: fatal error: no input files
compilation terminated.
configure:3335: $? = 4
configure:3324: gcc -qversion >&5
gcc: error: unrecognized option '-qversion'
gcc: fatal error: no input files
compilation terminated.
configure:3335: $? = 4
configure:3355: checking whether the C compiler works
configure:3377: gcc conftest.c >&5
configure:3381: $? = 0
configure:3429: result: yes
configure:3432: checking for C compiler default output file name
configure:3434: result: a.out
configure:3440: checking for suffix of executables
configure:3447: gcc -o conftest conftest.c >&5
configure:3451: $? = 0
configure:3473: result:
configure:3495: checking whether we are cross compiling
configure:3503: gcc -o conftest conftest.c >&5
configure:3507: $? = 0
configure:3514: ./conftest
configure:3518: $? = 0
configure:3533: result: no
configure:3538: checking for suffix of object files
configure:3560: gcc -c conftest.c >&5
configure:3564: $? = 0
configure:3585: result: o
configure:3589: checking whether we are using the GNU C compiler
configure:3608: gcc -c conftest.c >&5
configure:3608: $? = 0
configure:3617: result: yes
configure:3626: checking whether gcc accepts -g
configure:3646: gcc -c -g conftest.c >&5
configure:3646: $? = 0
configure:3687: result: yes
configure:3704: checking for gcc option to accept ISO C89
configure:3768: gcc -c -g -O2 conftest.c >&5
configure:3768: $? = 0
configure:3781: result: none needed
configure:3812: checking for style of include used by make
configure:3840: result: GNU
configure:3866: checking dependency style of gcc
configure:3977: result: gcc3
configure:3992: checking for gcc option to accept ISO C99
configure:4141: gcc -c -g -O2 conftest.c >&5
conftest.c:61:29: error: expected ';', ',' or ')' before 'text'
conftest.c: In function 'main':
conftest.c:115:18: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'newvar'
conftest.c:115:18: error: 'newvar' undeclared (first use in this function)
conftest.c:115:18: note: each undeclared identifier is reported only once for each function it appears in
conftest.c:125:3: error: 'for' loop initial declarations are only allowed in C99 mode
conftest.c:125:3: note: use option -std=c99 or -std=gnu99 to compile your code
configure:4141: $? = 1

andyturk
Associate II
August 29, 2012
Posted on August 29, 2012 at 20:34

Well, let's back up.... Is there some reason you don't want to use the built-in .cfg for that board?

$ openocd -f board/stm32f4discovery.cfg

Open On-Chip Debugger 0.6.0-rc1-dev-00015-g47728f9-dirty (2012-08-28-15:48)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.sourceforge.net/doc/doxygen/bugs.html

1000 kHz

srst_only separate srst_nogate srst_open_drain

Info : clock speed 1000 kHz

Info : stm32f4x.cpu: hardware has 6 breakpoints, 4 watchpoints

usafape
usafapeAuthor
Associate II
August 30, 2012
Posted on August 30, 2012 at 03:01

Hey,

That works!!! It must have been something done wrong in the .cfg file.

Thanks