UM2407 describes the different modes of solder bridges, including that of SB52:
- SB52=ON: VBAT pin of STM32H7 is connected to VDD_MCU.
- SB52=OFF: VBAT pin of STM32H7 is not connected to VDD_MCU.
The data sheet of the STM32H723 says about VBAT:
To optimize battery duration, this power domain is supplied by VDD when available or by the voltage applied on VBAT pin (when VDD supply is not present). VBAT power is switched when the PDR detects that VDD dropped below the PDR level.
The voltage on the VBAT pin could be provided by an external battery, a supercapacitor or directly by VDD, in which case, the VBAT mode is not functional.
So to use the VBAT function, you must open SB52 and supply VBAT accordingly.
Does it answer your question?
Regards
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.