Skip to main content
Icont.1
Associate III
November 9, 2021
Question

nucleo144 stm32h7a3 with custom board

I would like to use the stlink/v3 on the Nucleo144 stm32h7a3 board to program/debug my board is this possible? what do I need to connect?

This topic has been closed for replies.

4 replies

Chloe Meunier
ST Employee
November 9, 2021

Hello,

I advise you to download the nucleo board schematic to know witch connections are used. Board reference is MB1363 you can download schematics here: MB1363 - Resources - Search STMicrocontrollers

Connector CN5 is an easy way to connect a board to STLinkV3.

BR

Chloé

Icont.1
Icont.1Author
Associate III
November 9, 2021

I used the cn2 in this way from the left 3v3, swclk, gnd, swdio towards the pins of my card pin 3 (swclk), pin 1 (gnd), pin 4 (swdio) and pin 6 (3v3). when I connect it to debug to my program it tells me no device found on target

Chloe Meunier
ST Employee
November 9, 2021

You also need UART to work. signals T_VCP_TX and T_VCP-RX are available on CN5 connector.

TDK
November 9, 2021

I don't see an easy way on that board to disconnect SWDIO/SWCLK from the onboard processor. You would need to do that before using it to program an external board. The VCP connections are definitely optional.

"If you feel a post has answered your question, please click ""Accept as Solution""."