Skip to main content
Sco
ScoBest answer
ST Employee
Apr 2, 2026 1:38 AM UTC

NUCLEO-U3C5ZI-Q | Product - STMicroelectronics

the UM3599 has been uploaded. FYI.

9 replies

mƎALLEm
ST Technical Moderator
Mar 26, 2026 11:42 AM UTC

Hello, 

I will ask internally for for the user manual availability for that board.

Internal ticket number for follow-up: CDM0061050

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Pavel A.
Mar 30, 2026 3:10 AM UTC

In my very humble opinion, documentation for Nucleo boards is bad, and this begins already at the product page in the main ST website. Descriptions are generic, fuzzy, send the user around many hoops to discover the characteristics of the board. User needs to quickly see what a specific board provides, including properties of the specific MCU and other components on the board: size of flash, RAM, etc. without downloading and browsing numerous PDFs.

Couldn't they get some spare AI agents to write decent product info pages?

 

CTapp.1
CTapp.1Author
Senior III
Mar 30, 2026 1:46 PM UTC

For example, it would be really useful to have a single page showing all of the board that shows:

  1. Which transceivers are available on board (CAN, LIN, ...).
  2. Are any 8 or 16 bit wide ports available?
  3. Which peripherals have all their pins available on the various headers, which have reduced capability (half duplex, ...).
  4. ...
All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)
EZHON.1
ST Employee
Mar 30, 2026 1:10 AM UTC

Refer to the schematic is best to find which IO you want.

Pavel A.
Mar 31, 2026 3:04 AM UTC

I've tried to ask the Sidekick Screenshot 2026-03-31 055816.png about features of specific Nucleo board and it seems to know. It scanned the relevant PDFs and gives references. Would be cool if this thing were available on the whole site.

 

 

mƎALLEm
ST Technical Moderator
Apr 1, 2026 10:03 AM UTC

The request is already under analysis under the internal ticket CDM0061050

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Sco
ScoBest answer
ST Employee
Apr 2, 2026 1:38 AM UTC

NUCLEO-U3C5ZI-Q | Product - STMicroelectronics

the UM3599 has been uploaded. FYI.

CTapp.1
CTapp.1Author
Senior III
Apr 2, 2026 7:23 AM UTC

Thanks for the update and the fast response :)

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)