Skip to main content
Dick Mincher
Associate III
November 8, 2019
Question

Nucleo-L4A6ZG failure to program

I've just installed the latest version of STMCubeIDE on a Mac and am trying to flash a simple program generated by the IDE. I have installed the L4 pack.

The firmware on the ST-LINK has been updated.

I have no other ST boards and I am not sure if it is an issue with the processor support or my installation.

I get a "Problem Occured" popup with the details:

Error in final launch sequence:
 
Failed to execute MI command:
load /Users/****/STM32CubeIDE/workspace_1.0.2/Try3/Debug/Try3.elf 
 
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load /Users/****/STM32CubeIDE/workspace_1.0.2/Try3/Debug/Try3.elf 
 
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load /Users/****/STM32CubeIDE/workspace_1.0.2/Try3/Debug/Try3.elf 
 
Error message from debugger back end:
Error finishing flash operation
Error finishing flash operation

When I enable the GDB debug output I get . the following. Notice lines 47-48.

STMicroelectronics ST-LINK GDB server. Version 5.3.2
Copyright (c) 2019, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
 Persistent Mode : Disabled
 LogFile Name : /Users/****/STM32CubeIDE/workspace_1.0.2/Try3/Debug/st-link_gdbserver_log.txt
 Logging Level : 31
 Listen Port Number : 61234
 Status Refresh Delay : 15s
 Verbose Mode : Enabled
 SWD Debug : Enabled
 
Target connection mode: Attach
Hardware watchpoint supported by the target 
COM frequency = 4000 kHz
ST-LINK Firmware version : V2J34M25
Device ID: 0x461
PC: 0x1000000
ST-LINK device status: RUN_MODE
ST-LINK detects target voltage = 3.25 V
ST-LINK device status: RUN_MODE
ST-LINK device initialization OK
Waiting for debugger connection...
Waiting for connection on port 61234...
Accepted connection on port 61234...
Debugger connected
Try halt ...
ST-LINK device status: HALT_MODE
Enter STM32_AppReset() function 
NVIC_DFSR_REG = 0x00000009
NVIC_CFGFSR_REG = 0x00000000
XPSR = 0x01000000
 ------ Switching to STM32CubeProgrammer ----- 
[36m[01m -------------------------------------------------------------------
[39;49m[36m[01m STM32CubeProgrammer v2.2.0 
[39;49m[36m[01m -------------------------------------------------------------------
 
[39;49m[39;49m
 
[39;49m[39;49mLog output file: /tmp/STM32CubeProgrammer_O3bfOt.log
[39;49m[39;49m[39;49m[39;49m[90mST-LINK SN : 0671FF393430533457012229
[39;49m[90mST-LINK FW : V2J34M25
[39;49m[90mVoltage : 3.25V
[39;49m[90mSWD freq : 4000 KHz
[39;49m[90mConnect mode: Under Reset
[39;49m[90mReset mode : Hardware reset
[39;49m[90mCannot identify the device
[39;49m[00;31mError: unknown or unsupported device (DevID = 0x0000)
[39;49m[39;49m
 
[39;49m[39;49mMemory Programming ...
[39;49m[39;49mOpening and parsing file: ST-LINK_GDB_server_i7QNkR.srec
[39;49m[39;49m File : ST-LINK_GDB_server_i7QNkR.srec
[39;49m[39;49m Size : 9184 Bytes
[39;49m[39;49m Address : 0x08000000 
[39;49m[39;49m
 
[39;49m[39;49m[39;49mErasing memory corresponding to segment 0:
[39;49m[39;49m[39;49mDownload in Progress:
[39;49m[39;49m[39;49m[39;49m[39;49m[39;49m[00;32m[==================================================] 100% 
[39;49m[39;49m[39;49m
 
[39;49m[00;32mFile download complete
[39;49m[39;49mTime elapsed during download operation: 00:00:00.071
[39;49m[39;49m
 
[39;49m[39;49m
Verifying ...
[39;49m[39;49m
 
[39;49m[39;49mRead progress:
[39;49m[39;49m[39;49m[00;32m[=========== ] 22% 
[39;49m[39;49m
 
[39;49mError: Data mismatch found at address 0x08000000 (byte = 0x38 instead of 0x00)
[39;49m[39;49m
 
[39;49m[00;31mError: Download verification failed
[39;49m[39;49m
 
[39;49mEncountered Error when opening /Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.macos64_1.1.0.201910081157/tools/bin/STM32_Programmer_CLI
 ------ Switching context ----- 
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...

Any suggestions on how to resolve this?

Thank you for your help.

This topic has been closed for replies.

2 replies

Cartu38 OpenDev
Graduate II
November 8, 2019

According numerous post about sounds CubeProgrammer issue on MacOS. ST-Link GDB server is relying on so ...

In sync. with some other post get a try relying on OpenOCD probe … sounds such is working better (not relying on CubeProgrammer flash feature). Drawback about is some debug features are not OpenOCD supported. Up to you ...

Dick Mincher
Associate III
November 14, 2019

I converted the onboard ST-LINK to a JLINK per the Segger instructions and it works fine. I've worked around the issue for now, but there must be an issue either with the driver or my installation.