Skip to main content
picatostas
Associate II
Sep 29, 2020 4:54 PM UTC
Solved

NUCLEO-L031K6 ST-link is not being recognized

I have recently purchased a NUCLEO-L031K6 dev board and when connecting it via USB ST-Link won't get recognized. I have 2 other st-link which work like a charm, so drivers are there (STM Discovery F0 and ST-Link V2). Any help? Is there any boot sequence to follow for the ST-Link on the NUCLEO-L031K6 to be recognized ?

This topic has been closed for replies.
TDK
TDKBest answer
Sep 29, 2020 5:11 PM UTC

Nothing special about the board. Make sure you're not using a charging cable (without data lines connected).

"If you feel a post has answered your question, please click ""Accept as Solution""."

5 replies

ST Technical Moderator
Sep 29, 2020 5:09 PM UTC

Hello @picatostas​ ,

Have you tried using STM32CubeProg tool ?

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
picatostas
Associate II
Sep 29, 2020 5:34 PM UTC

Yes I tried first with that !

TDK
TDKBest answer
Sep 29, 2020 5:11 PM UTC

Nothing special about the board. Make sure you're not using a charging cable (without data lines connected).

"If you feel a post has answered your question, please click ""Accept as Solution""."
picatostas
Associate II
Sep 29, 2020 5:34 PM UTC

Good point, kind of shameful if my first post here is such a noob mistake :E

picatostas
Associate II
Sep 29, 2020 5:38 PM UTC

it was that indeed. Thanks! Happy Coding!