Nucleo-H755 ST-LINK MCU overheating and ST-LINK not detected
- 2 replies
- 265 views
Hello,
I am using an STM32H755 Nucleo board in a system where the board is plugged into a custom PCB via headers. The system has been working for about two weeks without any issues. Occasionally I remove the Nucleo board to update the firmware and then plug it back into the PCB.
Today the system stopped responding to UART commands. When I connected the board to my PC, STM32CubeIDE reported:
"No ST-LINK detected! Please connect ST-LINK and restart the debug session."
I also tried STM32 ST-LINK Utility and got:
"Can not connect to target! Please select 'Connect Under Reset' mode..."
However, STLinkUpgrade is able to detect the ST-LINK and perform a firmware upgrade.
Another important observation:
The ST-LINK MCU on the board (STM32F7) is getting very hot.
Additional diagnostics:
- The board was completely removed from the external PCB.
- Even when powered independently, the ST-LINK MCU still overheats.
- The board draws significantly higher current than normal.
- I cannot measure proper 3V or 5V rails on the board.
Because of these symptoms, I suspect the on-board ST-LINK MCU may be damaged.
Has anyone experienced a similar issue or can confirm if this behavior indicates a failed ST-LINK hardware?
Thank you.