Skip to main content
Visitor II
Jan 22, 2025 10:45 AM UTC
Solved

NUCLEO-H743ZI2 Fault LED is always ON

Hello,

I hope you are doing great, I am facing the issue with NUCLEO-H743ZI2 Board, The LD6 is always ON and the IC U2 is getting overheated as soon as we connect the USB cable to dump the code and also unable to dump the code. It would be great if someone resolve the issue, Thanks for your attention.

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jan 22, 2025 11:07 AM UTC

Hello @Rohith1 and welcome to the community,

Not easy to give you an answer if you didn't tell what you did before that behavior to occur.

The heating means you have a hardware issue / shortcut etc.. may be you've broken something on the board may be in the power block.

On which part of the board the overheating is released?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jan 22, 2025 11:07 AM UTC

Hello @Rohith1 and welcome to the community,

Not easy to give you an answer if you didn't tell what you did before that behavior to occur.

The heating means you have a hardware issue / shortcut etc.. may be you've broken something on the board may be in the power block.

On which part of the board the overheating is released?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.