NUCLEO-H723ZG OVRCR LED turns ON only when JP4 (VDD_MCU) is installed
- 1 reply
- 390 views
Hello everyone,
I am facing a persistent OVRCR (LD6) over-current indication on a NUCLEO-H723ZG board and would appreciate guidance.
Board behavior
Powering the board via CN1 (ST-LINK USB) only
No external connections: no peripherals, no wires, no common ground, no shields
Power source selector JP2 set to STLINK
Observations
JP4 removed (VDD_MCU / IDD link open):
LD6 (OVRCR) OFF
LD5 solid green
ST-LINK enumerates correctly on PC
E5V ≈ 5 V
3V3 ≈ 3.2–3.3 V
JP4 installed:
LD6 (OVRCR) turns RED immediately
LD5 flickers faintly
USB power switch (U2 near CN1) starts heating
Board does not stay powered
Current measurement across JP4:
Measured by replacing JP4 with a multimeter (DC current mode)
Target domain draws ~1 A
This happens regardless of JP5 position (VB–VDD or VDD–3V3)
Resistance measurements (USB unplugged):
With JP4 installed:
3V3 → GND ≈ 10–60 Ω
IOREF / VBAT → GND similar range
With JP4 removed:
3V3 / IOREF / VBAT → GND ≈ 150–200 Ω
Conclusion so far
Base power system is OK
Overcurrent occurs only when the VDD_MCU domain is connected
~1 A draw is far beyond normal for a bare target MCU domain
USB power switch correctly enters protection (OVRCR)
Questions
What is the expected current range for the VDD_MCU domain on NUCLEO-H723ZG at power-up?
Are there any known failure modes or checks recommended when:
OVRCR triggers immediately with JP4 installed
JP5 selection does not change behavior
Is there any additional jumper or configuration that could cause this behavior, or does this indicate a fault in the target power domain?
Any insights from ST or community members would be greatly appreciated.
Thank you.