Nucleo-H5E5ZJ Virtual com port documentation wrong.
In the UM3601 documentation 7.3.5. it mentions:
Virtual COM port
The USART1 serial interface (PD8/PD9) is directly available as a Virtual COM port of the PC connected to the
STLINK-V3EC USB connector (CN1).
However the PD8 and PD9 of this controller are UART3 NOT UART1.
Seems STM bringing out many Nucleo boards without reviewing documentation and without adding board specific out of the box working examples demonstrating the features of the processor and/or the board.