Skip to main content
TJM
Senior II
November 16, 2023
Solved

Nucleo-h563zi factory onboard example applicatio

I'm experimenting with the nucleo-h563zi board again using the examples in CubeIDE and CubeMX but I would like to end up replacing the LED/UserButton application that was originally installed when I received the board.  Can't find it.  Can someone point me in the right direction as to where the original firmware code or binary is located?  I've submitted this question a while back and the solution was to download the original firmware binary using CubeProgrammer.  Unfortunately, it's now too late for that.  This is the firmware where the three LEDs flash in order and the speed of the sequence increases with each push of the User Button.

Thanks for the assist.

TJM

This topic has been closed for replies.
Mike_ST
Mike_STBest answer
ST Technical Moderator
November 17, 2023

Hello

Here it is,

Download, unzip, and flash it at 0x8000000.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 

2 replies

Mike_ST
Mike_STBest answer
ST Technical Moderator
November 17, 2023

Hello

Here it is,

Download, unzip, and flash it at 0x8000000.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
TJM
TJMAuthor
Senior II
November 17, 2023

Thanks.  You guys are fast.

It would be nice if they included this firmware code in the CubeH5 package.  It appears there are several functions involved in this firmware that could be of interest to us while learning the board.

Thanks again,

TJM