Skip to main content
Gaston
Associate III
June 17, 2022
Question

NUCLEO-G031K8 using external 5V power supply issue

Hi,

I'm powering my NUCLEO-G031K8 from external 5V (LD2 led is On as expected) but the MCU stays in reset state (Vnrst=1.32V). I've changed the NRST_MODE to 1 (Reset Input only) with no success. The embedded ST-LINK is driving the MCU reset but in this case is not powered (USB disconnected).

How can I fix it?

regards,

gaston

This topic has been closed for replies.

4 replies

ST Employee
June 17, 2022

Hello Gaston,

No chance to remove this NRST connection from ST-Link thanks to a solder bridge ?

Regards,

Antoine

Gaston
GastonAuthor
Associate III
June 20, 2022

Hello Antoine,

No, no chance. I've already checked schematics. I will have to power the board through the USB connector.

gaston

Visitor II
August 6, 2024

Hey Antoine,

I feel that I've just faced the same issue. In this nucleo Board there is no way to disconnect properly µC NRST pin from ST Link. Thus, when I only wanted to supply the µC by the 3.3V port, the ST-link was not supplied (as wanted) and acted as a current sink disabling the NRST pin to reach 3.3V (it was stuck around 1.3V). I had to cut the track manually and everything worked fine.

Best regards,

Valentin

Mike_ST
ST Technical Moderator
August 6, 2024

Hello, thank you for the feedback.

I have entered a ticket in our database (#188171),

just in case, a new version of the PCB is made.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.