Skip to main content
iw2lsi
Associate III
March 29, 2019
Question

NUCLEO-F767ZI unable to do a FullChipErase

  • March 29, 2019
  • 8 replies
  • 1362 views

Hi,

i was playing with OptionBytes on my custom USB-Bootloader and... I end up in a bricked NUCLEO board... the CPU itself is still running (I can even update an application) but I cannot connect via ST-LINK and/or DfuSe anymore...

The error message is:

09:12:27 : Can not connect to target!

         If you're trying to connect to an STM32W1xx device, please select Normal or HotPlug mode from Target->Settings menu.

         If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu.

09:12:28 : No target connected

On the device folder:

DETAILS.TXT

------------------

Version: 0221

Build:  Sep 18 2018 11:09:21

FAIL.TXT

------------

The interface firmware FAILED to reset/halt the target MCU

ST-Link utils is v4.3.0.0

ST-LinkUSB-Driver is v5.1.0.0

ST-Link CLI is v3.3.0.0

The option "connect under reset" & pressing the B2 (reset) button before doing a chip erare seems not to work... somewhere there is a note regarding SB111 (pad between NRST-RST) but in my case a 0 ohm resistor is already there.

Any ideas on how to unbrick my NUCLEO board ?

thanks,

Giampaolo

This topic has been closed for replies.

8 replies

Uwe Bonnes
Chief
March 29, 2019

Try connect under reset or USB DFU.

iw2lsi
iw2lsiAuthor
Associate III
March 29, 2019

Hi Uwe...

I've already done this... and it did not work... I think I'm somehow in Level 2 protection:

Level 2 is an irreversible operation. When Level 2 is activated, the level of protection cannot be decreased to Level 0 or Level 1.

Giampaolo

AvaTar
Senior III
March 29, 2019

> Try connect under reset or USB DFU

Booting into system mode, and try a mass-erase there ?

Not sure if this is meant to be the same.

> I think I'm somehow in Level 2 protection:

>Level 2 is an irreversible operation. When Level 2 is activated, the level of protection cannot be decreased to Level 0 or Level 1.

Then you have bricked it probably ...

iw2lsi
iw2lsiAuthor
Associate III
March 29, 2019

uh...

I was convinced that full chip erase was always possible... but it seems that I was wrong... my bad.

Giampaolo

Uwe Bonnes
Chief
March 29, 2019

There are hacks out there that that will turn Level 2 into level 1. Look at the CC (Computer Chaos ) Club conferences talks. In short, they turn on the chip and turn off at the right moment. But buying a new Nucleo is much less effort.

iw2lsi
iw2lsiAuthor
Associate III
March 29, 2019

Hello Uwe...

.. I was also thinking at replacing the MCU... but since it costs $13 while the whole board is $20... it's a nonsense...

I've done a search for CCC and STM32 Level 2 but got nothing... do you have a link to the paper you are talking about ? I'm just curious....

tnx

Giampaolo

Uwe Bonnes
Chief
March 29, 2019
iw2lsi
iw2lsiAuthor
Associate III
March 29, 2019

amazing!

tnx Uwe...