Skip to main content
Explorer
Jul 30, 2026 4:17 PM UTC
Solved

NUCLEO-F767ZI, switching power supply as external source

 

Hi, looking to power the NUCLEO-F767ZI off another board (which has a TPSM843320 buck), any issues with this as the 5V rail (E5V), on the dev board you have LD1117 LDO, but the rail I can provide isn’t high enough for the dropout. 

 

Any spec on ripple or how clean the E5V rail should be? Seems to only be used by STLINK and USB.

FBLBest answer
ST Technical Moderator
Jul 31, 2026 2:08 PM UTC

Hi ​@HowMakeWork 

If your external rail on E5V can fall below 4.75 V, it is not considered acceptable for the E5V input.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

1 reply

FBLBest answer
ST Technical Moderator
Jul 31, 2026 2:08 PM UTC

Hi ​@HowMakeWork 

If your external rail on E5V can fall below 4.75 V, it is not considered acceptable for the E5V input.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL