Skip to main content
Associate III
August 15, 2023
Solved

nucleo-f410RB uart problem

I have nucleo-f410rb on hand
i tried to connect all three uart pin on the board (uart 1,2,6)
none of them work

and i found if i use keil to code the board, the uart2 message could come out from arduino board uart pin

but if i used STM32CubeIDE , it can't even come out from arduino board uart pin

i searched for this problem.

some said it is the problem of the division of uart clock(since i can see the message when keil is used, i don't think it is related)

 

what is the problem?

This topic has been closed for replies.
uveuvenouveBest answer
Associate III
August 15, 2023

seems my uart to usb device somehow not match stm32
i changed to a device use ch340 and now work

1 reply

uveuvenouveAuthorBest answer
Associate III
August 15, 2023

seems my uart to usb device somehow not match stm32
i changed to a device use ch340 and now work