Skip to main content
Andrew Neil
Super User
Nov 13, 2026 4:58 PM UTC
Question

Nucleo-C5A3ZG misleading LED documentation

UM3616 Rev 2:

 

That paragraph should be indented under LD2 & LD3 as it refers to only those 2 LEDs - not to LD1

In addition, it would be better to make it explicit: “LD2 & LD3 are OFF when the STM32 I/O is in a high state, and ON when the STM32 I/O is in a low state”

Better yet, add an explicit note that this is opposite to LD1!

“LD2 & LD3 are OFF when the STM32 I/O is in a high state, and ON when the STM32 I/O is in a low state. Note that this is opposite to LD1”

 

PS:

It would also be helpful to add “Active high” on LD1 and “Active low” on LD2 & 3 in Table 7:
 

 

1 reply

Mike_ST
ST Technical Moderator
Nov 16, 2026 3:02 PM UTC

Hello Andrew,

Thank you, a ticket has been entered in our database.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.