Skip to main content
SSara.11
Associate
September 27, 2020
Question

No target found error

Hi,

I am using STM32 controller (STM32L475VC) for our project. I am getting error as "NO TARGET FOUND" when

  1. I am trying to debug through ST-Link V2 or
  2. Trying to access the controller for Erase/Program with STM32CubeProgrammer

I have done following steps to erase & program the controller

  • Hold Reset pin low momentarily while connecting to target with STM32CubeProgrammer over SWD interface using ST-Link. Not able to access the target.
  • Tried to connect to target using "Under Reset" mode over SWD interface using ST-Link. Not able to access the target.
  • Put controller in USB DFU bootloder mode and able to erase & reprogram the controller successfully over USB interface using STM32CubeProgrammer. But again when I tried to debug/erase/program the controller over SWD interface using ST-link, I am getting same error as "NO TARGET FOUND"

Kindly, provide support for this issue.

Regards,

Sanjay

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
September 27, 2020

Has it every worked? custom board?

Pins not wired properly, buffers on ST-LINK/V2 not powered properly, see pin 1/2

Conflicting with other devices connected to SWDIO/SWCLK

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
SSara.11
SSara.11Author
Associate
September 28, 2020

Yes it was working Custom board.  Pins are wired properly. SWDIO/SWCLK pin are not conflicting with others