Skip to main content
Associate
Dec 16, 2025 7:48 PM UTC
Question

Ninebot GT2p control board nRST pin diagram

Hi does anybody know how to locate the nRST, pin on a GT2p, control board? When I connect st link it says UR connection needs SWrst which says I need to find the nRST, pin.  to connect another wire that goes from St link, v2, clone

to the nRST,  pin or button on the GT2p, control board. I can take a picture of what the PCB, looks like in about an hour? Thanks

4 replies

TDK
Dec 16, 2025 7:53 PM UTC

First identify the chip and look at the datasheet to see which pin is NRST.

On commercial products, the chip may be locked in RDP level 2 in which case ST-Link will be unable to connect. Contact the manufacturer to find out that info.

What are you trying to do?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
Dec 17, 2025 3:55 AM UTC

Stm32F405 I’m trying to change the

serial number to a Chinese serial number so I have all the bells and whistles and lights 

 

TDK
Dec 19, 2025 4:24 PM UTC

> Stm32F405 I’m trying to change the serial number to a Chinese serial number

Do you know how to do that? Have others done it and reported success? If it's a region-locked thing, the manufacturer probably did something to avoid this.

Hold BOOT0 high during reset (and BOOT1 low), connect to the chip using GND/SWDIO/SWCLK in STM32CubeProgrammer. If it doesn't work, the chip is either locked out or you've made an error in wiring. Since I don't physically have the board, not much else I can help with here.

"If you feel a post has answered your question, please click ""Accept as Solution""."